Property (Read-Write)
SCPI.TRIGger.OUTPut.SELect = Value
Value = SCPI.TRIGger.OUTPut.SELect
This command sets/gets external trigger output timing selection.
|
Parameter |
Value |
|
Description |
External trigger output timing selection |
|
Data Type |
Character string type (String) |
|
Range |
EOM|INDex |
|
Preset Value |
EOM |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "EOM"
SCPI.TRIGger.OUTPut.SELect = Var
Var = SCPI.TRIGger.OUTPut.SELect
PN Menu: Trigger > Ext Trig Output > Selection
SP Menu: Trigger > Ext Trig Output > Selection
FP Menu: Trigger > Ext Trig Output > Selection
TR Menu: Trigger > Ext Trig Output > Selection
AM Menu: Trigger > Ext Trig Output > Selection
BB Menu: Trigger > Ext Trig Output > Selection
:TRIGger:OUTPut:SELect {EOM|INDex}
:TRIGger:OUTPut:SELect?
{EOM|INDex} <newline><^END>
10 OUTPUT 717;":TRIGger:OUTPut:SELect EOM"
20 OUTPUT 717;":TRIGger:OUTPut:SELect ?"
30 ENTER 717;A$