Other topics about Setting Control Functions
You can save the instrument state of the E5052B into a file in the mass storage, and then recall it with the preset function to reproduce that state.
If no user preset instrument state is stored, you cannot set the user preset function.
Press Preset key.
Use one of the following keys for the desired setting:
|
Softkey |
Function |
|
Factory |
Specifies the normal preset function. |
|
User |
Specifies the user-preset function. |
|
Cancel |
Returns to the softkey display in one upper level. |
To execute the user-preset function, you must have a preset setting file that has been saved with the state at AutoRec.
When AutoRec is not stored, the softkey of "User Preset" is not activated (Gray-out). For more details on saving procedure refer to File Saving and Loading Instrument Status Settings.