The transient measurement has two measurement modes: Wide and Narrow. Wide band can observer the frequency transition in wider window.
Narrow band can observe the transient measurement of frequency, power and phase vs. time in narrower window.
Configure Transient Sweep settings |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Sweep Type Wide-Narrow- Wideband (WB) and one narrow band (NB1) measurements Narrow-Narow - two narrow band measurements, Narrow band 1 (NB1) and Narrow band 2 (NB2). Both bands are identical.
Time Coupling - All traces for both measurement share the same time settings. NOP - Shows the number of Point in the transient sweep. NOP is automatically set and cannot be changed. Wide
Narrow1/Narrow2
Note: Displayed area (time and frequency) needs to be set to keep frequency transient within NB1 Center Freq +- NB1 Freq Span / 2. Otherwise, a user will see an invalid trace. The same applies to Narrow band 2. Displayed area needs to be set to keep frequency transient within NB2 Center Freq +- NB2 Freq Span / 2. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||
Transient sweep can measure two different bands’ parameters simultaneously and each band’s NOP will be set automatically depending on parameter settings (band span/range, VBW, timespan). To display these different, NOP parameters on the same display window, Linear interpolation will be performed for some Transient parameters. Here is the rule of NOP/interpolation.
Band1 NOP < Band2 NOP: Band2 NOP is applied to Band 1 NOP with an linear interpolation.
Band1 NOP > Band2 NOP: Band1 NOP is applied to Band 2 NOP with an linear interpolation.
Wide Band NOP = Narrow Band1 NOP: No change on NOP operation.
Band 1/2 definition
Wide-Narrow mode
Band1: Wide band
Band2: Narrow band 1
Narrow-Narrow mode
Band1: Narrow band 1
Band2: Narrow band 2
Example
1) Wide band NOP: 1251, Narrow band 1 NOP: 626,
NOP of WB_Freq stays at 1251.
The NOP of NB1_Freq / NB1_Power / NB1_Phase is changed to 1251 with an linear interpolation.
2) Narrow band1 NOP: 1251, Narrow band 2 NOP: 10001,
The NOP of NB1_Freq/NB1_Power/NB1_Phase is changed to 10001 with an linear interpolation..
NOP of NB2_Freq / NB2_Power / NB2_Phase stays at 10001.
Enable Video Trigger - Enable the Video Trigger function. Select Trigger - Select the trigger source from Wide, Narrow1 or Narrow2. Trigger Type - Select Frequency or Power. Power is available in Narrow band only. Target - Target value which make a video trigger Hysteresis -
Hysteresis triggers eliminate incorrect triggers caused by noisy
signals. For example, if your signal contains several rising edges
of different amplitudes, you can use hysteresis triggering to
trigger on one of the edges. Edge - Select the trigger edge from positive or negative. Min Input Level - Minimum power input level for the video trigger. The relative value (dB) from the maximum input level should be specified. The trigger is disabled when the narrow band power measurement level is below the specified value. This does not work when the frequency span is 80 MHz and above because the power measurement is not available in the spans.
Holdoff -
An trigger insensitive period after the previous trigger. The
trigger is disabled during this period, even if the trigger conditions
are met.
|
|