Only the Main Power commands corresponding to the Phase Noise measurement class are documented here. The Port Power and Attenuators commands are identical to the Port Power and Attenuator commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtab on the graphic below.
Click here to view links to Power commands for all Measurement Classes.
| Main Tab Commands | |||
| Softkey | Sub-item | SCPI | COM |
| Power Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude]
DISPlay:GUI:POWer:SPIN:RESolution |
TestPortPower PowerSpinResolution |
|
| RF Power | ON/OFF | OUTPut[:STATe] | SourcePortMode |
|
|||
|
|||