Controls two output functions: RF power and Noise Source.
OUTPut: | [:STATe] |
Click on a red keyword to view the command details.
See Also
Example Programs
Applicable Models: All (Read-Write) Turns RF power from the source ON or OFF. See note about source power state with instrument state save and recall. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - turns RF power ON OFF (or 0) - turns RF power OFF |
Examples |
OUTP
ON |
Query Syntax |
OUTPut[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|