Selects a measurement parameter.
CALCulate:MEASure
|
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-Write) Set/get a measurement parameter for the specified (cnum/mnum) measurement. This command replaces the following commands: CALC:CUST:MOD
Note: For Application Measurements see CALCulate:MEASure:DEFine |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optinal). |
<mnum> |
Measurement number for each measurement. |
<string> |
Refer to measurement name in CALC:MEAS:DEF as a measurement parameter. |
Examples |
CALC:MEAS:PAR "Sdd11" calculate2:measure2:parameter "Sdd11" CALC:MEAS2:DEF 'PN:Phase Noise' 'Defines
a Phase Noise measurement but doesn't display. |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:PARameter? |
Return Type |
String |
"S11" |
|