Performs and applies Port Extensions.
SENSe:CORRection:EXTension: AUTO | CONFig | DCOFfset | LOSS | MEASure | PORT | RESet | STARt | STOP RECeiver | [TIME] |
Click on a keyword to view the command details.
See Also
Example Programs
Applicable Models: All (Read-Write) Sets the frequencies used to calculate Automatic Port Extension. Learn more about calculating Automatic Port Extension. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<char> |
Frequencies to be used: CSPN Use current frequency span. AMKR - Use active marker frequency. USPN - Use custom user span. Use SENS:CORR:EXT:AUTO:STAR and SENS:CORR:EXT:AUTO:STOP to specify start and stop frequency. |
Examples |
SENS:CORR:EXT:AUTO:CONF
CSPN |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:AUTO:CONFig ? |
Return Type |
Character |
CSPN |
|
Applicable Models: All (Read-Write) Specifies whether or not to include DC Offset as part of automatic port extension. Learn more about Automatic DC Offset. Only allowed when SENS:CORR:EXT:AUTO:LOSS is set to ON. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
ON (or 1) - Includes DC Offset correction. OFF (or 0) - Does NOT include DC Offset correction. |
Examples |
SENS:CORR:EXT:AUTO:DCOF
1 |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:AUTO:DCOFfset? |
Return Type |
Boolean |
ON (1) |
|
Applicable Models: All (Read-Write) Specifies whether or not to include loss correction as part of automatic port extension. Learn more about Loss Compensation in port extension. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
ON (or 1) - Includes Loss correction. OFF (or 0) - Does NOT include Loss correction. |
Examples |
SENS:CORR:EXT:AUTO:LOSS
1 |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:AUTO:LOSS? |
Return Type |
Boolean |
ON (1) |
|
Applicable Models: All (Write-only) Measures either an OPEN or SHORT standard. When this command is sent, the VNA acquires the measurement with which to set automatic port extensions. This command should be preceded by the CALCulate:PARameter:MNUMber <num> where num is the trace number of a measurement on the specified channel. Learn more about which standard to measure. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<char> |
Standard to be measured. Choose from: OPEN Measure OPEN standard SHORt Measure SHORT standard |
Examples |
SENS:CORR:EXT:AUTO:MEAS
OPEN |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Enables and disables automatic port extensions on the specified port. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<n> |
VNA Port number to enable or disable for automatic port extensions. |
<bool> |
ON (or 1) - Enable OFF (or 0) - Disable |
Examples |
SENS:CORR:EXT:AUTO:PORT2
0 |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:AUTO:PORT<n>? |
Return Type |
Boolean |
All ports ON (enabled) |
|
Applicable Models: All (Write-only) Clears old port extension delay and loss data in preparation for acquiring new data. Send this command prior to sending a new series of SENS:CORR:EXT:AUTO:MEAS. If acquiring both OPEN and SHORT standards, do not send this command between those acquisitions. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
Examples |
SENS:CORR:EXT:AUTO:RES |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Set the start frequency for custom user span. Learn more about User Span. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
User span start value. Must be within the frequency range of the active channel and less than the value set by SENS:CORR:EXT:AUTO:STOP. |
Examples |
SENS:CORR:EXT:AUTO:STAR
1E9 |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:AUTO:STARt <value>? |
Return Type |
Numeric |
Start frequency of the current active channel. |
|
Applicable Models: All (Read-Write) Set the stop frequency for custom user span. Learn more about User Span. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<value> |
User span stop value. Must be within the frequency range of the active channel and greater than the value set by SENS:CORR:EXT:AUTO:STARt |
Examples |
SENS:CORR:EXT:AUTO:STOP
1E9 |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:AUTO:STOP <value>? |
Return Type |
Numeric |
Stop frequency of the current active channel. |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets the extension value at the specified receiver. Must also set SENS:CORR:EXT ON. Note: Before using this command you must select a measurement using CALC:MEAS:DEFine. You can select one measurement for each channel. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<Rnum> |
Number
of the receiver that will receive the extension. If unspecified,
value is set to 1 1 for Receiver A 2 for Receiver B |
<num> |
The electrical length in seconds; may include
suffix. Choose a number between: |
Examples |
SENS:CORR:EXT:REC
2MS |
Query Syntax |
SENSe<cnum>:CORRection:EXTension:RECeiver<Rnum> [:TIME]? |
Return Type |
Numeric |
0 |
|