Controls the internal and external DC sources.
SOURce:DC: | AFC |FREQuency | BAND | INPut | LEVel | MAXimum | LIMit | HIGH | LOW | TABle | STATe | TARGet | CATalog? | CENTer | ENABle | LIMit | MAXimum | MINimum | LNOise | PARallel | SPAN | STARt | STATe | STOP |
Click on a keyword to view the command details.
Applicable Models: E505xA (Read-Write) Selects the frequency band which include the target VCO frequency. |
|
Parameters |
|
<range> |
R40M: 1 M - 40 MHz R1G5: 10 M - 1.5 GHz R8G: 250 M - 8 GHz RMAX: Max Freq. > 8 GHz |
Examples |
SOUR:DC:AFC:FREQ:BAND R1G5 source:dc:afc:frequency:band R40M |
Query Syntax |
:SOURce:DC:AFC:FREQuency? |
Return Type |
String |
R8G |
|
Applicable Models: E505xA (Write Only) Tune the frequency one time. |
|
Parameters |
|
Examples |
SOUR:DC:AFC:IMM source:dc:afc:immediate |
Query Syntax |
N/A |
Return Type |
N/A |
N/A |
|
Applicable Models: E505xA (Read-Write) |
|
Parameters |
|
<Boolean> |
|
Examples |
SOUR:DC:AFC:INP:LEV:MAX source:dc:afc:input:level:maximum |
Query Syntax |
:SOURce:DC:AFC:INPut:LEVel:MAXimum? |
Return Type |
|
|
|
Applicable Models: E505xA (Read-Write) Set and read the maximum number of readings to take at each data point for iterating the frequency. |
|
Parameters |
|
<value> |
the maximum number of iteration |
Examples |
SOUR:DC:AFC:ITER source:dc:afc:iteration |
Query Syntax |
:SOURce:DC:AFC:ITERation? |
Return Type |
Numeric |
10 |
|
Applicable Models: E505xA (Read-Write) Set and read the maximum limit of VControl during Auto Tune sequence. |
|
Parameters |
|
<value> |
The maximum limit of VControl |
Examples |
SOUR:DC:AFC:LIM:HIGH source:dc:afc:limit:high |
Query Syntax |
:SOURce:DC:AFC:LIMit:HIGH? |
Return Type |
Numeric |
18 |
|
Applicable Models: E505xA (Read-Write) Set and read the minimum limit of VControl during Auto Tune sequence. |
|
Parameters |
|
<value> |
The minimum limit of VControl |
Examples |
SOUR:DC:AFC:LIM:LOW source:dc:afc:limit:low |
Query Syntax |
:SOURce:DC:AFC:LIMit:LOW? |
Return Type |
Numeric |
0.5 |
|
Applicable Models: E505xA (Read-Write) Set and read the sensitivity of VCO (Hz/Volt). This value is used at the first loop of sequence. |
|
Parameters |
|
<value> |
Sensitivity in Hz/Volt |
Examples |
SOUR:DC:AFC:SENS source:dc:afc:sensitivity |
Query Syntax |
:SOURce:DC:AFC:SENSitivity? |
Return Type |
Numeric |
5E7 |
|
Applicable Models: E505xA (Read-Write) Set and read the sensitivity table of VCO. This value is used at the first loop of sequence. At least two points should be defined. If only one data is defined:
|
|
Parameters |
|
<value> |
volt0, freq0, volt1, freq1, volt2, freq2, ..... |
Examples |
SOUR:DC:AFC:SENS:TABL:DATA 0.8, 0.7E9, 0.9, 0.9E9, 1.1, 1.1E9, 1.2, 1.3E9 source:dc:afc:sensitivity:table:data 0.8, 0.7E9, 0.9, 0.9E9, 1.1, 1.1E9, 1.2, 1.3E9 |
Query Syntax |
:SOURce:DC:AFC:SENSitivity:TABle:DATA? |
Return Type |
array |
null |
|
Applicable Models: E505xA (Write Only) Clear the sensitivity table |
|
Parameters |
|
Examples |
SOUR:DC:AFC:SENS:TABL:DEL source:dc:afc:sensitivity:table:delete |
Query Syntax |
N/A |
Return Type |
N/A |
N/A |
|
Applicable Models: E505xA (Read-Write) Enable and disable the Auto Tune VControl voltage |
|
Parameters |
|
<Boolean> |
OFF / 0 ON / 1 |
Examples |
SOUR:DC:AFC:STAT ON source:dc:afc:state 1 |
Query Syntax |
:SOURce:DC:AFC:STATe? |
Return Type |
Boolean |
0 |
|
Applicable Models: E505xA (Read-Write) Set and read the target frequency. |
|
Parameters |
|
<value> |
The target frequency |
Examples |
SOUR:DC:AFC:TARG source:dc:afc:target |
Query Syntax |
:SOURce:DC:AFC:TARGet? |
Return Type |
Numeric |
1E6 |
|
Applicable Models: E505xA (Read-Write) Set and read the maximum desired deviation from the specified target frequency. |
|
Parameters |
|
<value> |
Tore lance value |
Examples |
SOUR:DC:AFC:TOL source:dc:afc:tolerance |
Query Syntax |
:SOURce:DC:AFC:TOLerance? |
Return Type |
Numeic |
1E5 |
|
Applicable Models: E505xA (Read-only) Returns the names of the configured and active DC sources for the specified channel. Use SYST:CONF:EDEV:CAT? to read a list of all configured external devices, including inactive devices. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
Examples |
SOUR:DC:CAT? 'Returns the following... "VControl,VSupply1,VSupply2" |
Return Type |
String, Names are separated by commas. |
Not Applicable |
|
Applicable Models: E505xA (Read-Write) Sets and returns center DC value for the specified DC source. This function is used to set the voltage even if the VContol or VSupply1/2 parameter is non swept. When the VContol or VSupply1/2 is not swept, use 0 for span. This value is changed automatically |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
<name> |
String. DC Source Name. See SOUR:DC:CAT? for selection. The upper/lower case letter must match. The name and port must EXACTLY match those in the DC Source Control dialog. |
<num> |
Center value. Choose a value within the range of the DC source. |
Examples |
SOUR2:DC:CENT "VSupply1",3 source:dc:center "VSupply1",1 |
Query Syntax |
SOURce<ch>:DC:CENTer? <name> |
Return Type |
Numeric |
5 |
|
Applicable Models: E5055A (Read-Write) Sets and returns the ON / Off state of all configured DC sources for the specified channel. Individual DC sources must ALSO be enabled using SOUR:DC:STATe. Use SOUR:DC:CAT? to read a list of ACTIVE configured DC source names E5055A: If one of channel is set at On in this command, the DC out is turned on. DC out is turned off only when all channels are set at Off. Use SYST:DC:ENABle to turn off DC output for all channels. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
<bool> |
ON / Off state. Choose from: ON or 1 - All DC sources enabled. OFF or 0 - All DC sources disabled. |
Examples |
SOUR:DC:ENAB 0 |
Query Syntax |
SOURce<ch>:DC:ENABle? |
Return Type |
Boolean |
1 |
|
Applicable Models: E505xA (Read-Write) Sets and returns the Max DC limit value for a DC source. |
|
Parameters |
|
<ch> |
This value is ignored. Same value is applied to all channel. |
<name> |
String. DC Source Name. See SOUR:DC:CAT? for selection. The upper/lower case letter must match. The name must EXACTLY match those in the DC Source Control dialog. |
<num> |
Max DC limit value. Choose a value within the range of the DC source. |
Examples |
SOUR2:DC:LIM:MAX "VControl",5 source:dc:limit:maximum "VControl",5 |
Query Syntax |
SOURce<ch>:DC:LIMit:MAXimum? <name> |
Return Type |
Numeric |
Depending on source |
|
Applicable Models: E505xA (Read-Write) Sets and returns the Min DC limit value for a DC source. |
|
Parameters |
|
<ch> |
This value is ignored. Same value is applied to all channel. |
<name> |
String. DC Source Name. See SOUR:DC:CAT? The upper/lower case letter must match. The name must EXACTLY match those in the DC Source Control dialog. |
<num> |
Min DC limit value. Choose a value within the range of the DC source. |
Examples |
SOUR2:DC:LIM:MIN "VSupply1",-2 source:dc:limit:minimum "VSupply2",-5 |
Query Syntax |
SOURce<ch>:DC:LIMit:MINimum? <name> |
Return Type |
Numeric |
Depending on source |
|
Applicable Models: E505xA (Read-Write) Enable and disable the low noise V Control. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
<device> |
String. "VControl". Specifying other devices will result error () |
<Boolean> |
Choose from: ON or 1 OFF or 0 |
Examples |
SOUR2:DC:LNO "VContorl",1 source:dc:lnoise "VContorl",0 |
Query Syntax |
SOURce<ch>:DC:LNOise? <device> |
Return Type |
String |
0 |
|
Applicable Models: E505xA (Read-Write) Sets and returns the ON / Off state of the specified DC Channel State. SOUR:DC:STAT should be turned ON. When SOUR:DC:STAT is OFF, No control is selected. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
<name> |
String. The name of DC Source. Choose from: The upper/lower case letter must match. VControl VSupply1 VSupply2 |
<statel> |
Choose from: ON OFF DEFault |
Examples |
SOURc:DC:OUTP "VControl", ON |
Query Syntax |
SOURce<ch>:DC:OUTPut? <name> |
Return Type |
Character |
DEF |
|
Applicable Models: E505xA (Read-Write) Parallel Mode. This command is to make a single aggregate port out of two power ports - specifying whether one result is same. |
|
Parameters |
|
<ch> |
This parameter is ignored. The setting is applied to all channels. |
<device> |
String. Choose from: VSupply1 VSupply2 |
<Boolean> |
Choose from: ON or 1 OFF or 0 |
Examples |
SOUR2:DC:PAR "VSupply1",1 source:dc:parallel "VSupply2",0 |
Query Syntax |
SOURce<ch>:DC:PARallel? <device> |
Return Type |
Boolean |
|
|
Applicable Models: E505xA (Read-only) Reads the DC source names |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
Examples |
SOUR:DC:NAM? |
Query Syntax |
SOURce<ch>:DC:NAMes? |
Return Type |
|
Not Applicable |
|
Applicable Models: E505xA (Read-Write) Sets and returns span value for the specified DC source. This function is used to set the voltage even if the VContol or VSupply1/2 parameter is non swept. When the VContol or VSupply1/2 is not swept, use 0 for span. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
<name> |
String. DC Source Name. See SOUR:DC:CAT? for selection. The upper/lower case letter must match. The name must EXACTLY match those in the DC Source Control dialog. |
<num> |
Span value. Choose a value within the range of the DC source. |
Examples |
SOUR2:DC:SPAN "VSupply1",3 source:dc:span "VSupply1",1 |
Query Syntax |
SOURce<ch>:DC:SPAN? <name[,port]> |
Return Type |
Numeric |
5 |
|
Applicable Models: E505xA (Read-Write) Sets and returns start DC value for the specified DC source. This function is used to set the voltage even if the VContol or VSupply1/2 parameter is non swept. When the VContol or VSupply1/2 is not swept, use the same voltage for both start and stop. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
<name> |
String. DC Source Name. See SOUR:DC:CAT? for selection. The upper/lower case letter must match. The name must EXACTLY match those in the DC Source Control dialog. |
<num> |
Start value. Choose a value within the range of the DC source. |
Examples |
SOUR2:DC:STAR "VSupply1",3 source:dc:start "VSupply1",1 |
Query Syntax |
SOURce<ch>:DC:START? <name[,port]> |
Return Type |
Numeric |
5 |
|
Applicable Models: E5055A (Read-Write) Sets and returns the ON / Off state of the specified DC source and port. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
<name> |
String. DC Source Name. See SOUR:DC:CAT? for selection. The upper/lower case letter must match. The name must EXACTLY match those in the DC Source Control dialog. |
<bool> |
ON / Off state. Choose from: ON or 1 - DC source/port enabled. OFF or 0 - DC source/port disabled. |
Examples |
SOUR:DC:STAT "VSupply1", 1 SOUR:DC:STAT? "VControl" |
Query Syntax |
SOURce<ch>:DC:STATe? <name[,port]> |
Return Type |
Boolean |
0 - OFF |
|
Applicable Models: E505xA (Read-Write) Sets and returns stop DC value for the specified DC source. This function is used to set the voltage even if the VContol or VSupply1/2 parameter is non swept. When the VContol or VSupply1/2 is not swept, use the same voltage for both start and stop. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
<name> |
String. DC Source Name. See SOUR:DC:CAT? for selection. The upper/lower case letter must match. The name must EXACTLY match those in the DC Source Control dialog. |
<num> |
Stop value. Choose a value within the range of the DC source. |
Examples |
SOUR2:DC:STOP "VSupply1",3 source:dc:stop "VSupply1",1 |
Query Syntax |
SOURce<ch>:DC:STOP?<name[,port]> |
Return Type |
Numeric |
0 |
|