Controls Receiver Leveling.
SOUR:POW:ALC[:MODE]: ACQuisition: | MODE ITERation | ENABle | VALue MODulation | APERture | OFFSet | SPAN | [:STATe] | BANDwidth | NOISe | MAX | MIN | STEP |
Click on a keyword to view the command details.
See Also
Example Programs
Remotely Specifying a Source Port
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets all ports to pre-sweep or point leveling mode for the specified channel. A channel cannot be set to both pre-sweep and point leveling. For point leveling, the source power is adjusted per point until the leveling receiver reports that the power is within tolerance (or the maximum iteration setting is reached). When the iteration is done, it moves immediately to the next point. This function is enabled using the SOURce:POWer:ALC[:MODE]:RECeiver:ITERation:ENABle command. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<char> |
Acquisition mode. Choose from: PRESweep - Leveling sweeps are performed in the background (not visible) before every measurement sweep to measure and apply source correction data. POINt - Source power is adjusted per point. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:ACQ:MODE PRES source2:power2:alc:mode:receiver:acquisition:mode presweep See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:ACQuisition:MODE? [src] |
Return Type |
Character |
PRESweep |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the state of a separate IFBW setting for leveling sweeps. ON allows a higher (faster) IFBW than the measurement sweep. It also causes leveling sweeps to be noisier. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
Separate IFBW setting state. ON or 1 - Separate IFBW setting. Specify IFBW using SOUR:POW:ALC:MODE:REC:IFBW OFF or 0 - Same IFBW as the measurement sweep. Specify IFBW using Sens:BWID |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:FAST 1 source2:power2:alc:mode:receiver:fast off source:power:alc:mode:receiver:fast off,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:FAST? [src] |
Return Type |
Boolean |
ON |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the frequency range to use for receiver leveling. On the user interface, this is the "Receiver frequency is determined by:" setting. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<char> |
Frequency range. Choose from: AUTO - always uses the frequency range that is assigned to the measurement receiver. INPut - Mixer/Converter input frequency range. OUTPut - Mixer/Converter input frequency range. RECeiver - FOM Receiver frequency range. SOURce - FOM Source frequency range |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:FTYP AUTO source2:power2:alc:mode:receiver:ftype input source:power:alc:mode:receiver:ftype output,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:FTYPe? [src] |
Return Type |
Character |
AUTO |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the IFBW to be used for leveling sweeps. Enable separate IFBW for leveling sweeps using SOUR:POW:ALC:MODE:REC:FAST 1 |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling..If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
IFBW for leveling sweeps in Hz. The list of valid IF Bandwidths is different depending on the VNA model. (Click to see the lists.) If an invalid number is specified, the analyzer will round up to the closest valid number. This parameter supports MIN and MAX as arguments. Learn more. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:IFBW 100E3 source2:power2:alc:mode:receiver:ifbw 100khz source:power:alc:mode:receiver:ifbw 70e3,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:IFBW? [src] |
Return Type |
Numeric |
100 kHz |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Enables or disables the receiver leveling maximum iteration search function set using the SOURce:POWer:ALC[:MODE]:RECeiver:ACQuisition:MODE. The maximum iterations are set using the SOURce:POWer:ALC[:MODE]:RECeiver:ITERation:VALue command. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
Safe mode state. ON or 1 - Enable receiver leveling maximum iteration search. OFF or 0 - Disable receiver leveling maximum iteration search. The prior value for maximum iterations is retained. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:ITER:ENAB 1 source2:power2:alc:mode:receiver:iteration:enable on source:power:alc:mode:receiver:iteration:enable off,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:ITERation:ENABle? [src] |
Return Type |
Boolean |
ON |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the maximum iterations to be used in order to achieve the tolerance setting. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Max iterations. Choose a value 0 to 50. Note: Entering a value of 0 is allowed and sets the receiver leveling to Prior-Sweep mode. Learn more. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:ITER:VAL 5 source2:power2:alc:mode:receiver:iteration:value 10 source:power:alc:mode:receiver:iteration:value 7,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:ITERation:VALue? [src] |
Return Type |
Numeric |
10 |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the state of Use Last Result for Source Power Cal. When Leveling Mode is switched back to Internal, this feature turns Source Power Cal correction ON using the latest receiver leveling correction data. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
State of Use Last Result for Source Power Cal. ON or 1 - When Leveling Mode is switched back to Internal, Source Power Cal correction is turned ON using the latest receiver leveling correction data. OFF or 0 - When Leveling Mode is switched back to Internal, Source Power Cal correction is NOT turned ON. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:LSPC 1 source2:power2:alc:mode:receiver:lspc off source:power:alc:mode:receiver:lspc off,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:LSPC? [src] |
Return Type |
Boolean |
OFF |
|
Applicable Models: N524xB with S93070xB, and/or N522xB, N523xB, N524xB with S9x09xxA/B, S9x090A/B, M98xxA/P50xxA with 090/190 + S9x090B and/or S95070xA/B (M98xxA only) (Read-Write) Sets and returns the offset of the frequency aperture used to measure the signal power. Since the ideal modulation signal is known, the total power is calculated from this value. The SOURce:POWer:ALC:MODE:RECeiver:MODulation:APERture:STATe must be set to ON to enable this setting. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Receiver leveling aperture offset in Hz. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:MOD:APER:OFFS 1E6 source2:power2:alc:mode:receiver:modulation:aperture:offset 1E6,"MXG_Vector" |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:MODulation:APERture:OFFSet? [src] |
Return Type |
Numeric |
0 |
|
Applicable Models: N524xB with S93070xB, and/or N522xB, N523xB, N524xB with S9x09xxA/B, S9x090A/B, M98xxA/P50xxA with 090/190 + S9x090B and/or S95070xA/B (M98xxA only) (Read-Write) Sets and returns the span of the frequency aperture used to measure the signal power. Since the ideal modulation signal is known, the total power is calculated from this value. The SOURce:POWer:ALC:MODE:RECeiver:MODulation:APERture:STATe must be set to ON to enable this setting. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Receiver leveling aperture span in Hz. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:MOD:APER:SPAN 10e6 source2:power2:alc:mode:receiver:modulation:aperture:span 10e6,"MXG_Vector" |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:MODulation:APERture:SPAN? [src] |
Return Type |
Numeric |
10e6 |
|
Applicable Models: N524xB with S93070xB, and/or N522xB, N523xB, N524xB with S9x09xxA/B, S9x090A/B, M98xxA/P50xxA with 090/190 + S9x090B and/or S95070xA/B (M98xxA only) (Read-Write) Sets and returns the state of the receiver leveling aperture settings for the specified source for Modulation Distortion measurements. Enabling the aperture settings will measure the power more quickly by reducing the span of the measurement. Enter the span and offset of the frequency aperture used to measure the signal power. Since the ideal modulation signal is known, the total power is calculated from this value. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
State of receiver leveling aperture settings. ON or 1 - Enable span and offset aperture settings. OFF or 0 - Disable span and offset aperture settings. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:MOD:APER 1 source2:power2:alc:mode:receiver:modulation:aperture:state 1,"MXG_Vector" |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:MODulation:APERture[:STATe]? [src] |
Return Type |
Boolean |
OFF |
|
Applicable Models:N524xB with S93070xB, and/or N522xB, N523xB, N524xB with S9x09xxA/B, S9x090A/B, M98xxA/P50xxA with 090/190 + S9x090B and/or S95070xA/B (M98xxA only) (Read-Write) Sets and returns the receiver noise bandwidth value for the specified source for Modulation Distortion measurements. Noise bandwidth is equal to the Resolution bandwidth divided by the Vector Average factor. The SOURce:POWer:ALC:MODE:RECeiver:FAST command must be set to ON to enable this setting. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Noise bandwidth value in Hz. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:MOD:BAND:NOIS 1e3 source2:power2:alc:mode:receiver:modulation:bandwidth:noise 1e3,"MXG_Vector" |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:MODulation:BANDwidth:NOISe? [src] |
Return Type |
Numeric |
1000 |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the power level offset value. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Power level offset in dB. Choose a value between +200 and -200. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:OFFS 10 source2:power2:alc:mode:receiver:offset 5 source:power:alc:mode:receiver:offset 7,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:OFFSet? [src] |
Return Type |
Numeric |
0 |
|
Applicable Models: N522xB, N523xB, N524xB (Read-only) Returns the receiver ratio to be used with receiver leveling. This receiver ratio parameter is the same as the one set in SOUR:PHAS:PARameter. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:RAT 10 source2:power2:alc:mode:receiver:ratio "a1/a3,3" source:power:alc:mode:receiver:ratio "R1/R3,3","Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:RATio? [src] Returned is two VNA physical receivers that are controlled by different sources and the port that is 'paired' with <port>. The receivers and paired port are separated by a comma. |
Return Type |
String |
"a1/a3,3" |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the reference receiver to be used with Receiver Leveling. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<rec> |
(String) VNA receiver. Choose the VNA physical receiver that works with the source port <port>. For example:<port 1> = "R1" |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:REF 'r1' source2:power2:alc:mode:receiver:reference 'r2' source:power:alc:mode:receiver:reference "r1","Port 1 Src2" 'Read the last setting back source:power:alc:mode:receiver:reference? "Port 1 Src2" 'Returns: "R1,1" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:REFerence? [src] |
Return Type |
String - Name of the reference receiver. |
Not Applicable |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the state of Safe Mode. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
Safe mode state. ON or 1 - Safe mode ON OFF or 0 - Safe mode OFF |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:SAFE 1 source2:power2:alc:mode:receiver:safe on source:power:alc:mode:receiver:safe:state off,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:SAFE[:STATe]? [src] |
Return Type |
Boolean |
OFF |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the maximum power level for Safe Mode. The MAX/MIN limit is always used regardless of the safe mode state. In addition, the MAX/MIN limit is for port power and related to power offset. If the power offset is not set correctly, the MAX/MIN limit is not correct and it may impact the leveling. Ensure that the power offset in the channel is the same as power offset during calibration. If the exact power offset is not known, choose a limit for source and then it will not be related to power offset. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Maximum power level in dB. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:SAFE:MAX 10 source2:power2:alc:mode:receiver:safe:max 20 source:power:alc:mode:receiver:safe:max 15,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:SAFE:MAX? [src] |
Return Type |
Numeric |
30 dB |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the minimum power level for Safe Mode. The MAX/MIN limit is always used regardless of the safe mode state. In addition, the MAX/MIN limit is for port power and related to power offset. If the power offset is not set correctly, the MAX/MIN limit is not correct and it may impact the leveling. Ensure that the power offset in the channel is the same as power offset during calibration. If the exact power offset is not known, choose a limit for source and then it will not be related to power offset. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Minimum power level in dB. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:SAFE:MIN -50 source2:power2:alc:mode:receiver:safe:min -80 source:power:alc:mode:receiver:safe:min -40,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:SAFE:MIN? [src] |
Return Type |
Numeric |
-95 dB |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the maximum step power level for Safe Mode. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Maximum Step power level in dB. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:SAFE:STEP 2 source2:power2:alc:mode:receiver:safe:step 1.5 source:power:alc:mode:receiver:safe:min 2,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:SAFE:STEP? [src] |
Return Type |
Numeric |
1 dB |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the state of Receiver Leveling for the specified source port. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<bool> |
Receiver Leveling state. ON or 1 - Receiver Leveling ON OFF or 0 - Receiver Leveling OFF |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC 1 source2:power2:alc:mode:receiver on source:power:alc:mode:receiver:state off,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver[:STATe]? [src] |
Return Type |
Boolean |
OFF |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and returns the tolerance value for leveling sweeps. |
|
Parameters |
|
<ch> |
Channel number to be receiver leveled. If unspecified, value is set to 1 |
<port> |
Source port being used for Receiver Leveling. If unspecified, value is set to 1. To make settings for ports that are not simple numbers, use the [src] argument. |
<value> |
Tolerance level in dB. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SOUR:POW:ALC:REC:TOL .01 source2:power2:alc:mode:receiver:tolerance .5 source:power:alc:mode:receiver:tolerance .2,"Port 1 Src2" See ReceiverLeveling example |
Query Syntax |
SOURce<ch>:POWer<port>:ALC[:MODE]:RECeiver:TOLerance? [src] |
Return Type |
Numeric |
.1 dB |
|