Contains the settings to configure a "Cal All" Calibration.
Use the Guided Cal interface to perform the calibration.
SYSTem:CALibrate:ALL: CHANnel: CSET: | CATalog? GUIDed: | PORTs? INDependent: | SOURce: | CALibration: | CATalog? | RANGe: | ADD | CLEar | COUNt | PONts | STARt | STOP MCLass: | PROPerty: | VALue: | CATalog? | [STATe] PATH: | CONFigure: | ELEMent PORT<n>: | SOURce:POWer: | ATTen | OFFSet | [VALue]
|
Click on a red keyword to view the command details.
See Also
Applicable Models: E505xA with VNA ports (Write-Read) For each channel to be calibrated, sets and returns the ports to be calibrated. Specify port numbers ONLY for standard channels. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<ch> |
Channel number to be calibrated. |
<value> |
Ports to be calibrated for the specified channel. Select any of the native VNA ports (1,2,3,4). |
Examples |
SYST:CAL:ALL:CHAN2:PORT 1,2,3 |
Query Syntax |
SYSTem:CALibrate:ALL:CHANnel<ch>:PORTs[:SELect]? |
Return Type |
Comma-separated port numbers. |
1,2 |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns the User Cal Set or cal register names that were produced by the cal all session. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
Examples |
SYST:CAL:ALL:CSET:CATalog? 'returns this format: "MyCalAll_STD_001, MyCalAll_SMC_002" |
Return Type |
String of comma-separated Cal Set or cal register names |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the prefix to be used when saving User Cal Sets that result from the Cal All session. The Meas Class and channel number are appended to this prefix for each calibrated channel. Use SYST:CAL:ALL:CSET:CATalog? to read the saved cal set names.
|
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<value> |
(String) User Cal Set prefix. |
Examples |
SYST:CAL:ALL:CSET:PREFix "MyCalAll" |
Query Syntax |
SYSTem:CALibrate:ALL:CSET:PREFix? |
Return Type |
String |
" " (Empty string) |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns all cal all guided calibration channels. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
Examples |
chan = SYST:CAL:ALL:GUID:CHAN:LIST? |
Return Type |
Numeric of comma-separated channel numbers |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns the primary guided calibration channel number if more than one channel exists; otherwise, this command returns the one value. Use this value as the <ch> argument for the subsequent Guided:Cal commands. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
Examples |
chan = SYST:CAL:ALL:GUID:CHAN:VAL? |
Return Type |
Numeric |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns the ports to be calibrated during the Cal All Channels calibration. Specify connectors and cal kits for these ports using the Guided:Cal commands. Specify the ports to be calibrated for each channel using SYST:CAL:ALL:CHAN<ch>:PORT. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
Examples |
ports = SYST:CAL:ALL:GUID:PORT? |
Return Type |
Comma-separated list of port numbers |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the IFBW for a Cal All calibration. Learn more about this setting. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<value> |
IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the VNA model. See the list of valid settings. If an invalid number is specified, the VNA will round up to the closest valid setting. This command supports MIN and MAX as arguments. Learn more. |
Examples |
SYST:CAL:ALL:IFBW 10e3 |
Query Syntax |
SYSTem:CALibrate:ALL:IFBW? |
Return Type |
Numeric |
1 kHz |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns available ports for independent power calibration. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
Examples |
SYST:CAL:ALL:IND:SOUR:CAL:CAT? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: E505xA with VNA ports (Write-only) This command adds a power cal range for a specific port <n>. Note that external sources are valid and specifying a source port is the same as other remote commands. By default this will create a range with the preset start/stop frequency and 201 points. The maximum number of ranges that can be added is 100 (same as the maximum number of segments). |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Port number |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG:ADD |
Default |
Not applicable |
Applicable Models: E505xA with VNA ports (Write-only) This command resets all ranges for the given source port <n>. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Port number |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG:CLE |
Default |
Not applicable |
Applicable Models: E505xA with VNA ports (Read-only) This command queries how many ranges are included in the calibration for source port <n>. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Port number |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG:COUN? |
Return Type |
Numeric |
Default |
Not applicable |
Applicable Models: E505xA with VNA ports (Write-Read) This command sets and gets the number of points for range <m> for source port<n>. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Port number |
<m> |
Range number |
<value> |
Number of points |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG1:POIN 7 |
Query Syntax |
SYSTem:CALibrate:ALL:INDependent:SOURce<n>:CALibrate:RANGe<m>:POINts? |
Return Type |
Numeric |
Default |
201 |
Applicable Models: E505xA with VNA ports (Write-Read) This command sets and gets the start frequency for range <m> for source port<n>. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Port number |
<m> |
Range number |
<value> |
Start frequency for range <m> |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG1:STAR 20e9 |
Query Syntax |
SYSTem:CALibrate:ALL:INDependent:SOURce<n>:CALibrate:RANGe<m>:STARt? |
Return Type |
Numeric |
Default |
Not applicable |
Applicable Models: E505xA with VNA ports (Write-Read) This command sets and gets the stop frequency for range <m> for source port<n>. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Port number |
<m> |
Range number |
<value> |
Stop frequency for range <m> |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG1:STOP 21e9 |
Query Syntax |
SYSTem:CALibrate:ALL:INDependent:SOURce<n>:CALibrate:RANGe<m>:STOP? |
Return Type |
Numeric |
Default |
Not applicable |
Applicable Models: E505xA with VNA ports (Read-only) Returns the unique, settable properties for the current cal all session. See a list of valid properties and values for each measurement class. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
[mclass] |
Optional argument. String name of the measurement class for which properties are to be returned. See a list of valid measurement class Application names. The measurement class must be included in the current Cal All calibration. |
Examples |
SYST:CAL:ALL:MCL:PROP:NAME:CAT? 'with NFX app, returns: "Noise Cal Method,Noise Tuner,AutoOrient Tuner,Tuner In,Tuner Out,Receiver Characterization Method,ENR File,Noise Source Connector,Noise Source CalKit" |
Return Type |
String of comma-separated properties. |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns the valid property values for a specific property name. See a list of valid properties and values for each measurement class. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<prop> |
(String) Property name for which valid values are to be returned. |
Examples |
SYST:CAL:ALL:MCL:PROP:VAL:CAT? "Noise Cal Method" 'with NFX app, returns: "Scalar,Vector" |
Return Type |
String of comma-separated values |
Not applicable |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the property value for a specific property name. See a list of valid properties and values for each measurement class. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<prop> |
(String) Property name for which value is to be set or returned. |
<value> |
Property value. To read a list of valid values, use SYST:CAL:ALL:MCL:PROP:VAL:CAT? |
Examples |
Example
1: Example 2: Example 3: |
Query Syntax |
SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue[:STATe]? <prop> |
Return Type |
String |
Varies with the property name. |
|
Applicable Models: N522xB, N523xB, N524xB, M983xA (Write-Read) Sets and returns the Path Configuration settings for a Cal All calibration. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<element> |
(String) Path configuration element to be set. See a list of configurable RF Path elements and settings. |
<setting> |
(String) Path configuration element setting. |
Examples |
SYST:CAL:ALL:PATH:CONFigure:ELEMent "Port1NoiseTuner","Internal" |
Query Syntax |
SYSTem:CALibrate:ALL:PATH:CONFigure:ELEMent[:STATe]? <element> |
Return Type |
String |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the Receiver Attenuator setting for a Cal All calibration. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Receiver port number. |
<value> |
Attenuation value in dB for a Cal All calibration. Choose a valid value for the VNA model. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:REC:ATT 10 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:RECeiver:ATTen? |
Return Type |
Numeric |
0 |
|
Applicable Models: N522xB, N523xB, N524xB, M9485A
(Write-Read) Sets and returns the reference attenuator setting for a Cal All calibration. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Receiver port number. |
<num> |
Attenuation value in dB for a Cal All calibration. 0dB or 35dB. If a number other than these is entered, the analyzer will select the next lower valid value. For example, if 19dB is entered, then 0dB attenuation will be selected. |
Examples |
SYST:CAL:ALL:PORT2:REC:ATT:REF 0 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:RECeiver:ATTen:REFerence? |
Return Type |
Numeric. If querying for the standard (M9376A) port, the return value is 0 |
35 |
|
Applicable Models: N522xB, N523xB, N524xB, M9485A
(Write-Read) Sets and returns the test attenuator setting for a Cal All calibration. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Receiver port number. |
<num> |
Attenuation value in dB for a Cal All calibration. 0dB or 35dB. If a number other than these is entered, the analyzer will select the next lower valid value. For example, if 19dB is entered, then 0dB attenuation will be selected. |
Examples |
SYST:CAL:ALL:PORT2:REC:ATT:TEST 0 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:RECeiver:ATTen:TEST? |
Return Type |
Numeric. If querying for the standard (M9376A) port, the return value is 0. |
35 |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Write-Read) Sets and returns the Source Attenuator setting for the Cal All calibration. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Source port number. |
<value> |
Attenuation value in dB for the Cal All calibration. Choose a valid value for the VNA model. See valid settings. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:SOUR:POW:ATT 10 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:SOURce:POWer:ATTen? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the power offset value for a Cal All calibration. Power Offset provides a method of compensating port power for added attenuation or amplification in the source path. The result is that power at the specified port reflects the added components. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Source port number. |
<value> |
Power offset value in dB for a Cal All calibration.
|
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:SOUR:POW:OFFS 10 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:SOURce:POWer:OFFSet? |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the power level at which a Cal All calibration is to be performed. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<n> |
Source port number. |
<value> |
Power level at which the calibration is to be performed. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source outputs on the 2-port PNA-X model with multiple sources such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:SOUR:POW 0 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:SOURce:POWer[:VALue]? |
Return Type |
Numeric |
Preset power of the VNA model. See the data sheet for the power level for each model. |
|
Applicable Models: E505xA with VNA ports (Write-only) Resets all properties associated with the Cal All session to their default values. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
Examples |
SYST:CAL:ALL:RES |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Write-Read) Sets and returns the list of channels to be calibrated during the Cal All session. |
|
Parameters |
|
[1-250] |
Calibration number. The default is 1. |
<value> |
Channel numbers to be calibrated. These channels must already exist. |
Examples |
SYST:CAL:ALL:SEL 1,2,3 |
Query Syntax |
SYSTem:CALibrate:ALL:SELect? |
Return Type |
Comma-separated channel numbers. |
Existing channels |
|