User Accounts and Passwords


Important: When the analyzer power is switched on, it AUTOMATICALLY logs into Windows using the default user name and password. You do NOT need to log on.  This gives anyone full access to the analyzer. The following steps can be taken to increase security of your analyzer

Please read about Anti-virus protection for your analyzer.

Existing User Accounts

The following user accounts already exist on new SSAs.

Important: For the highest security, it is recommended to change the passwords on your device from these defaults.

User Name

Password

Type

Description

Instrument

Keysight4u!

Administrator

Auto Log On is activated by default.

Administrator

Keysight4u!

Built-in Administrator

For user maintenance purpose.

Note: The user name is not case sensitive. The password is case sensitive.

Note: The local policies are set so that, if logon is required, you must retype the user name (and password) every time. Do not change the local policies on the analyzer.

Add or Change User Accounts, Passwords, and require Logon

If the analyzer is in a secure environment, you can setup users by name and grant various levels of access.

You can designate a person as the administrator and then configure the analyzer to allow others to use it with reduced permissions. That is, other people can be signed on to use the analyzer but they will not have the ability to perform all of the administrative functions that you can as the administrator.  

The following are examples of some of the functions that can be performed with these account types:

 

Windows 10

To add a new account:

Click Start > Settings > Accounts > Other people > Add someone else to this PC.

Enter the requested information then select Next.

To change an existing account:

Click on the user account.

Click Change account type.

Under Account type, select Standard User or Administrator.

Click OK.