Show 

Making DC Measurement at Sweep End (Option 3L5/3L4/3L3 only)

Other topics about Making Measurement

DC Measurement at end of sweep

E5061B option 3L5 allows you to measure DC level at the end of measurement sweep. When this function is turned on, after the sweep is finished, the DC level is measured in the condition of the last point of sweep, then result is displayed at the upper right corner of the screen.

  1. Press Meas > DC Monitor Setup.

  2. Click Function to select the port for DC measurement.

  3. Click DC Monitor Sweep End > Monitor to turn ON the DC monitor function.

  4. The result is displayed at the upper right corner of the screen.

Clear the DC measurement Data

You can clear the DC measurement data. This can be used when you want to clear the data at the hold status.

  1. Click Meas > DC Monitor Setup > DC Monitor Sweep End > Clear to reset the DC measurement at sweep end.