SCPI.INPut.IMPedance.GPPort.T

Object Type

Property (Read-Write)

Syntax

SCPI.INPut.IMPedance.GPPort.T = Value

Value = SCPI.INPut.IMPedance.GPPort.T

Description

This command sets/gets input impedance of port T for gain phase measurement.

Variable

Parameter

Value

Description

input impedance of port T

Data Type

Double precision floating point type (Double)

Range

50 or 1E+6

Preset Value

1E+6

Unit

Ω

Examples

Dim ImpPortT as Double
SCPI.INPut.IMPedance.GPPort.T = 1E+6
ImpPortT = SCPI.INPut.IMPedance.GPPort.T

Related Objects

SCPI.INPut.ATTenuation.GPPort.R

SCPI.INPut.ATTenuation.GPPort.T

SCPI.INPut.IMPedance.GPPort.R

Equivalent Key

Meas > Gain-Phase > T Input Z > 50Ω | 1MΩ

System > Overload Recovery > T Input Z > 50Ω | 1MΩ

Equivalent SCPI Command

Syntax

:INPut:IMPedance:GPPort:T <numeric>

:INPut:IMPedance:GPPort:T?

Query Response

{numeric} <newline><^END>

Example of use

10 OUTPUT 717;":INP:IMP:GPP:T 50"
20 OUTPUT 717;":INP:IMP:GPP:T?"
30 ENTER 717;A