Other topics about Using Windows
The E5061B has six USB ports for connecting devices: two in the front panel and four on the rear panel. The main advantages of USB are instant connect and disconnect, and faster data transfer speed. Electronic Calibration modules are now available with USB connections.
The first time you plug a device into a USB port there is some wait time. Windows reports that it is identifying the hardware, then searching for the correct driver, then installing the driver (if it is found).
Connecting that same device back into that same port later is quick and easy, but if you move the device to a different USB port, you will have to wait through the hardware ID and driver search again.
Certain USB devices (such as ECal modules) require you to be logged on with Administrator's privileges, the first time you plug them into the E5061B. This must be done for each serial number. Click Next to choose the default settings when installing new USB devices.
Some USB memory may not operate on the E5061B. In that case, try the other kind of USB memory. There is some USB memories which do not work on the front panel USB port, but work on the rear panel USB port.
Keysight Technologies shall not be responsible for, nor assume any liability for data loss in your USB memory device after using it with the E5061B.
Plug & Play capabilities provide both a stable and secured operating environment. You may also notice that it greatly reduces the number of required reboots.
Windows supports DHCP and fixed IP addressing. Also, instant connect and disconnect of the LAN cable, as well as a visual indicator of LAN status in system tray area, makes LAN connections more intuitive. In addition, the Hardware Wizard helps users with system hardware configuration.
By default, Windows allows a double-click method of launching icons. To revert to single-clicking, see the Windows help.
Adding a printer should be done as Windows operation. See Connecting Printer.