Command/Query
:CALCulate<Ch>[:SELected]:FUNCtion:PEXCursion <Value>
:CALCulate<Ch>[:SELected]:FUNCtion:PEXCursion?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:PEXCursion <Value>
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:PEXCursion?
This command sets/gets the limit of peak excursion.
|
Parameter |
Value |
|
Description |
Lower limit of peak excursion value |
|
Data Type |
Numeric type (Real) |
|
Range |
0 to 500M |
|
Preset Value |
3 |
|
Unit |
Varies depending on the data format.
|
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric}<newline><^END>
See Peak Search.
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.FUNCTION.PEXCURSION
SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.PEXCURSION