Command/Query
:CALCulate<Ch>[:SELected]:FUNCtion:TARGet <Value>
:CALCulate<Ch>[:SELected]:FUNCtion:TARGet?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:TARGet <Value>
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:TARGet?
This command sets/gets the target value when performing the target search with the :CALC:FUNC:EXEC.
|
Parameter |
Value |
|
Description |
Target value |
|
Data Type |
Numeric type (Real) |
|
Range |
-500M to 500M |
|
Preset Value |
0 |
|
Unit |
Varies depending on the data format. Log magnitude (MLOG) : dB (decibel) Phase (PHAS), Expanded phase (UPH) or Positive phase (PPH) : ° (degree) Group delay (GDEL) : s (second) Others : No unit |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric}<newline><^END>
See Peak Search.
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.FUNCTION.TARGET
SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.TARGET