Command/Query
:CALCulate<Ch>[:SELected]:FUNCtion:TTRansition {POSitive|NEGative|BOTH}
:CALCulate<Ch>[:SELected]:FUNCtion:TTRansition?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:TTRansition {POSitive|NEGative|BOTH}
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:TTRansition?
This command sets/gets the transition type when performing the target search with the :CALC:FUNC:EXEC.
|
Parameter |
Selection Option |
|
Description |
Transition type for search |
|
Data Type |
Character string type (String) |
|
Range |
"POSitive": Positive transition. "NEGative": Negative transition. "BOTH": Both the positive transition and the negative transition. |
|
Preset Value |
"BOTH" |
{POS|NEG|BOTH}<newline><^END>
See Peak Search.
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.FUNCTION.TTRANSITION
SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.TTRANSITION