MWA Operational Requirements

Requirements for operating the MWA software (Rev 1.1) are as follows:

A PC for running the front-end application

The ENA Network Analyzer (E5070B/E5071B/E5071C)

Multiport Test Set 

If you wish to make multiport measurements, the following multiport test sets are supported by the MWA.

ECal Module

When using the ECal module with calibration wizard in the back-end application of the MWA, the 4-port ECal module supported by the ENA is required. Refer to ECal for supported ECal modules by the ENA.

 

Other topics about Measurement Wizard Assistant