Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.BLIMit.DB = Value
Value = SCPI.CALCulate(Ch).SELected.BLIMit.DB
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).BLIMit.DB = Value
Value = SCPI.CALCulate(Ch).TRACe(Tr).BLIMit.DB
This command sets/gets the bandwidth threshold value (attenuation from the peak) of the bandwidth test, for the selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
In revision A.9.60 and above, you can select the trace and set/get the bandwidth threshold value for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
Bandwidth N dB points. |
|
Data type |
Double precision floating point type (Double) |
|
Range |
0 to 5E8 |
|
Preset value |
0 |
|
Unit |
dB |
For information on the variable (Ch), see Variable.
Dim BLimDB As Double
SCPI.CALCulate(1).SELected.BLIMit.DB = 3
BLimDB = SCPI.CALCulate(1).SELected.BLIMit.DB
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.BLIMit.STATe
Analysis > Bandwidth Limit > N dB Points
All revision:
:CALCulate{[1]-160}[:SELected]:BLIMit:DB <numeric>
:CALCulate{[1]-160}[:SELected]:BLIMit:DB?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:BLIMit:DB <numeric>
:CALCulate{[1]-160}:TRACe{[1]-16}:BLIMit:DB?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:BLIM:DB 3"
20 OUTPUT 717;":CALC1:BLIM:DB?"
30 ENTER 717;A