Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.BLIMit.STATe = Status
Status = SCPI.CALCulate(Ch).SELected.BLIMit.STATe
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).BLIMit.STATe = Value
Value = SCPI.CALCulate(Ch).TRACe(Tr).BLIMit.STATe
This command turns ON/OFF the bandwidth test function, for the active trace of selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
In revision A.9.60 and above, you can select the trace and turn ON/OFF the bandwidth test function for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
ON/OFF the bandwidth test function. |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
False or OFF |
For information on the variable (Ch), see Variable.
Dim BLimTest As Boolean
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.BLIMit.STATe = True
BLimTest = SCPI.CALCulate(1).SELected.BLIMit.STATe
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.BLIMit.DB
SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.MARKer
SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.VALue
SCPI.CALCulate(Ch).SELected.BLIMit.FAIL
SCPI.CALCulate(Ch).SELected.BLIMit.MAXimum
SCPI.CALCulate(Ch).SELected.BLIMit.MINimum
SCPI.CALCulate(Ch).SELected.BLIMit.REPort.DATA
Analysis > Bandwidth Limit > BW Test
All revision:
:CALCulate{[1]-160}[:SELected]:BLIMit[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}[:SELected]:BLIMit[:STATe]?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:BLIMit[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}:TRACe{[1]-16}:BLIMit[:STATe]?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:BLIM ON"
20 OUTPUT 717;":CALC1:BLIM?"
30 ENTER 717;A