Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.VALue = Status
Status = SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.VALue
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).BLIMit.DISPlay.VALue = Status
Value = SCPI.CALCulate(Ch).TRACe(Tr).BLIMit.DISPlay.VALue
This command turns ON/OFF the bandwidth value display of the bandwidth test, for the active trace of selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
In revision A.9.60 and above, you can select the trace and turn ON/OFF the bandwidth value display of the bandwidth tests for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
ON/OFF of the bandwidth display of the bandwidth test. |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following.
|
|
Preset value |
False or OFF |
For information on the variable (Ch), see Variable.
Dim BLimVal As Boolean
SCPI.CALCulate(1).PARameter(1).SELectSCPI.CALCulate(1).SELected.BLIMit.DISPlay.VALue = True
BLimVal = SCPI.CALCulate(1).SELected.BLIMit.DISPlay.VALue
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.BLIMit.STATe
SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.MARKer
Analysis > Bandwidth Limit > BW Display
All revision:
:CALCulate{[1]-160}[:SELected]:BLIMit:DISPlay:VALue {ON|OFF|1|0}
:CALCulate{[1]-160}[:SELected]:BLIMit:DISPlay:VALue?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:BLIMit:DISPlay:VALue {ON|OFF|1|0}
:CALCulate{[1]-160}:TRACe{[1]-16}:BLIMit:DISPlay:VALue?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:BLIM:DISP:VAL ON"
20 OUTPUT 717;":CALC1:BLIM:DISP:VAL?"
30 ENTER 717;A