Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.STATe = Status
Status = SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.STATe
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.DOMain.STATe = Status
Status = SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.DOMain.STATe
This command sets/gets whether to use an arbitrary range when executing the analysis with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object, for the selected channel (Ch).
When the trace coupling is off, the active trace is the target to be set.
In revision A.9.60 and above, you can select the trace and set/get whether to use an arbitrary range when executing the analysis with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object for the trace (when trace coupling is off) just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
Selection of the analysis range |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
False or OFF |
Dim AnaRnge As Boolean
SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STARt = 1.5E9
SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STOP = 1.8E9
SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STATe = True
AnaRnge = SCPI.CALCulate(1).SELected.FUNCtion.DOMain.STATe
SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.STARt
SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.STOP
SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.COUPle
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:FUNCtion:DOMain[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}[:SELected]:FUNCtion:DOMain[:STATe]?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:DOMain[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:DOMain[:STATe]?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:FUNC:DOM ON"
20 OUTPUT 717;":CALC1:FUNC:DOM?"
30 ENTER 717;A