Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.FUNCtion.PPOLarity = Param
Param = SCPI.CALCulate(Ch).SELected.FUNCtion.PPOLarity
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.PPOLarity = Param
Param = SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.PPOLarity
This command sets/gets the polarity when performing the peak search with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object, for the active trace of the selected channel (Ch).
In revision A.9.60 and above, you can select the trace and set/get the polarity when performing the peak search with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Param |
|
Description |
Polarity for peak search |
|
Data type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Preset value |
"POSitive" |
Dim PeakPol As String
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "peak"
SCPI.CALCulate(1).SELected.FUNCtion.PPOLarity = "both"
PeakPol = SCPI.CALCulate(1).SELected.FUNCtion.PPOLarity
SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE
SCPI.CALCulate(Ch).SELected.FUNCtion.PEXCursion
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:FUNCtion:PPOLarity {POSitive|
NEGative|BOTH}
:CALCulate{[1]-160}[:SELected]:FUNCtion:PPOLarity?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:PPOLarity {POSitive|
NEGative|BOTH}
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:PPOLarity?
{POS|NEG|BOTH}<newline><^END>
10 OUTPUT 717;":CALC1:FUNC:PPOL BOTH"
20 OUTPUT 717;":CALC1:FUNC:PPOL?"
30 ENTER 717;A$