Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.FUNCtion.TTRansition = Param
Param = SCPI.CALCulate(Ch).SELected.FUNCtion.TTRansition
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.TTRansition = Param
Param = SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.TTRansition
This command sets/gets the transition type when performing the target search with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object, for the active trace of the selected channel (Ch).
In revision A.9.60 and above, you can select the trace and set/get the transition type when performing the target search with the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Param |
|
Description |
Transition type for search |
|
Data type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Preset value |
"BOTH" |
Dim TargTran As String
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "atar"
SCPI.CALCulate(1).SELected.FUNCtion.TTRansition = "pos"
TargTran = SCPI.CALCulate(1).SELected.FUNCtion.TTRansition
SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE
SCPI.CALCulate(Ch).SELected.FUNCtion.TARGet
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:FUNCtion:TTRansition {POSitive|
NEGative|BOTH}
:CALCulate{[1]-160}[:SELected]:FUNCtion:TTRansition?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:TTRansition {POSitive|
NEGative|BOTH}
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:TTRansition?
{POS|NEG|BOTH}<newline><^END>
10 OUTPUT 717;":CALC1:FUNC:TTR NEG"
20 OUTPUT 717;":CALC1:FUNC:TTR?"
30 ENTER 717;A$