Property (Read Only)
All revision:
Data = SCPI.CALCulate(Ch).SELected.LIMit.REPort.ALL
In revision A.9.60 and above, the following syntax is also supported:
Data = SCPI.CALCulate(Ch).TRACe(Tr).LIMit.REPort.ALL
This command reads the bandwidth test results (stimulus value, limit test result, upper limit value and lower limit value of all measurement points), for the active trace of selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
In revision A.9.60 and above, you can select the trace and read the bandwidth test results for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Data |
|
Description |
Indicates the array data (for limit line) of NOP (number of measurement points)x4. Where n is an integer between 1 and NOP.
The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
For information on the variable (Ch), see Variable.
Dim LimData As Variant
SCPI.CALCulate(1).PARameter(1).SELect
LimData = SCPI.CALCulate(1).SELected.LIMit.REPort.ALL
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.LIMit.STATe
SCPI.CALCulate(Ch).SELected.LIMit.REPort.DATA
SCPI.CALCulate(Ch).SELected.LIMit.REPort.POINts
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:LIMit:REPort:ALL?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:LIMit:REPort:ALL?
10 OUTPUT 717;":SENS1:SWE:POIN?"
20 ENTER 717;A
30 REDIM B(1:4*A)
40 OUTPUT 717;":CALC1:LIM:REP:ALL?"
50 ENTER 717;B(*)