Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.LINE = Status
Status = SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.LINE
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.DISPlay.LINE = Status
Status = SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.DISPlay.LINE
This command turns ON/OFF the ripple limit line display, for the active trace (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command) of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and turn ON/OFF the ripple limit line display for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
ON/OFF the ripple limit line display. |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
False or OFF |
Dim RLimDisp As Boolean
SCPI.CALCulate(1).SELected.RLIMit.DISPlay.LINE = True
RLimDisp = SCPI.CALCulate(1).SELected.RLIMit.DISPLay.LINE
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.RLIMit.STATe
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.SELect
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.VALue
Analysis > Ripple Limit > Ripple Limit
All revision:
:CALCulate{[1]-160}[:SELected]:RLIMit:DISPlay:LINE {ON|OFF|1|0}
:CALCulate{[1]-160}[:SELected]:RLIMit:DISPlay:LINE?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:DISPlay:LINE {ON|OFF|1|0}
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:DISPlay:LINE?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:RLIM:DISP:LINE ON"
20 OUTPUT 717;":CALC1:RLIM:DISP:LINE?"
30 ENTER 717;A