Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.VALue = Param
Param = SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.VALue
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.DISPlay.VALue = Param
Param = SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.DISPlay.VALue
This command sets/gets the display type of ripple value for the active trace (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command)of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and set/get the display type of ripple value for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Param |
|
Description |
The displaying type of ripple value. |
|
Data type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Preset value |
"OFF" |
Dim RDisp As String
SCPI.CALCulate(1).SELected.RLIMit.DISPlay.VALue = "ABSolute"
RDisp = SCPI.CALCulate(1).SELected.RLIMit.DISPlay.VALue
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.RLIMit.STATe
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.LINE
SCPI.CALCulate(Ch).SELected.RLIMit.DISPlay.SELect
Analysis > Ripple Limit > Ripple Value > OFF|Absolute|Margin
All revision:
:CALCulate{[1]-160}[:SELected]:RLIMit:DISPlay:VALue {OFF|ABS|MAR}
:CALCulate{[1]-160}[:SELected]:RLIMit:DISPlay:VALue?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:DISPlay:VALue {OFF|ABS|MAR}
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:DISPlay:VALue?
{OFF|ABS|MAR}<newline><^END>
10 OUTPUT 717;":CALC1:RLIM:DISP:VAL ABS"
20 OUTPUT 717;":CALC1:RLIM:DISP:VAL?"
30 ENTER 717;A$