Property
All revision:
Data = SCPI.CALCulate(Ch).SELected.RLIMit.REPort.DATA
In revision A.9.60 and above, the following syntax is also supported:
Data = SCPI.CALCulate(Ch).TRACe(Tr).RLIMit.REPort.DATA
This command reads the ripple value of the ripple test for the active trace (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command)of selected channel (Ch).
The data transfer format when this command is executed depends on the setting with the SCPI.FORMat.DATA command.(Read only)
In revision A.9.60 and above, you can select the trace and read the ripple value of the ripple test for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Data |
|
Description |
Indicates the array data (for ripple line) of 1 + Num (number of limit lines)*3. Where n is an integer between 1 and 12.
The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
Dim RData As Variant
SCPI.CALCulate(1).PARameter(1).SELect
RData = SCPI.CALCulate(1).SELected.RLIMit.REPort.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.RLIMit.STATe
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:RLIMit:REPort[:DATA]?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:RLIMit:REPort[:DATA]?
{numeric 1},… ,{numeric 1+Nx3}<newline><^END>
|
Type |
Description |
|
<numeric 1> |
Number of ripple limit line (1 to 12) |
|
<numeric 1+(n\ 3)-2> |
Number of ripple limit bands |
|
<numeric 1+(n\ 3)-1> |
Ripple value |
|
<numeric 1+(n\ 3)> |
Results of ripple test 0: Pass 1: Fail |
Where N is the number of lines (specified with <numeric 1>) and n is an integer between 1 and 12.
10 DIM B(1:2,1:3)
20 OUTPUT 717;":CALC1:RLIM:REP?"
30 ENTER 717;A,B(*)