Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.TRANsform.TIME.CENTer = Value
Value = SCPI.CALCulate(Ch).SELected.TRANsform.TIME.CENTer
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).TRANsform.TIME.CENTer = Value
Value = SCPI.CALCulate(Ch).TRACe(Tr).TRANsform.TIME.CENTer
This command sets/gets the center value used for the transformation function of the time domain function, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and set/get the center value for the transformation function of the time domain function, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
Center value |
|
Data type |
Double precision floating point type (Double) |
|
Range |
Varies depending on the frequency span and the number of points. |
|
Preset value |
0 |
|
Unit |
s (second) |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Cent As Double
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.TRANsform.TIME.CENTer = 1E-8
Cent = SCPI.CALCulate(1).SELected.TRANsform.TIME.CENTer
SCPI.CALCulate(Ch).SELected.TRANsform.TIME.SPAN
SCPI.CALCulate(Ch).SELected.TRANsform.TIME.STATe
SCPI.CALCulate(Ch).PARameter(Tr).SELect
Analysis > Transform > Center
All revision:
:CALCulate{[1]-160}[:SELected]:TRANsform:TIME:CENTer <numeric>
:CALCulate{[1]-160}[:SELected]:TRANsform:TIME:CENTer?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:TRANsform:TIME:CENTer <numeric>
:CALCulate{[1]-160}:TRACe{[1]-16}:TRANsform:TIME:CENTer?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:TRAN:TIME:CENT 1E-8"
20 OUTPUT 717;":CALC1:TRAN:TIME:CENT?"
30 ENTER 717;A