Property (Read-Write)
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.OFFSet = Value
Value = SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.OFFSet
This command sets/gets the external signal source frequency is set by using an offset value for the basic frequency, for the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Setting of an offset value for the basic frequency |
|
Data type |
Double precision floating point type (Double) |
|
Range |
-1E12 to 1E12 |
|
Preset value |
0 |
|
Unit |
Hz (hertz) |
|
Resolution |
1 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Offset As Double
SCPI.SENSe(1).OFFSet.LOCal.FREQuency.OFFSet = -10
Offset = SCPI.SENSe(1).OFFSet.LOCal.FREQuency.OFFSet
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.DIVisor
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.MULTiplier
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STARt
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STOP
Sweep Setup > Frequency Offset > External Source > Offset
The basic frequency range is set by using “SCPI.SENSe(Ch).FREQuency.STARt” and “SCPI.SENSe(Ch).FREQuency.STOP”.
:SENSe{[1]-160}:OFFSet:LOCal[:FREQuency]:OFFSet <numeric>
:SENSe{[1]-160}:OFFSet:LOCal[:FREQuency]:OFFSet?
{numeric}<newline><^END>
10 OUTPUT 717;":SENS1:OFFS:LOC:OFFS 5E9"
20 OUTPUT 717;":SENS1:OFFS:LOC:OFFS?"
30 ENTER 717;A