Property (Read-Write)
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STOP = Value
Value = SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STOP
This command sets/gets a stop value for the external signal source frequency setting, for the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Setting of a stop value for the external signal source |
|
Data type |
Double precision floating point type (Double) |
|
Range |
0 to 1E12 |
|
Preset value |
0 |
|
Unit |
Hz (hertz) |
|
Resolution |
1 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Stop As Double
SCPI.SENSe(1).OFFSet.LOCal.FREQuency.STOP = 100E6
Stop = SCPI.SENSe(1).OFFSet.LOCal.FREQuency.STOP
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.DIVisor
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.MULTiplier
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.OFFSet
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STARt
Sweep Setup > Frequency Offset > External Source > Stop
:SENSe{[1]-160}:OFFSet:LOCal[:FREQuency]:STOP <numeric>
:SENSe{[1]-160}:OFFSet:LOCal[:FREQuency]:STOP?
{numeric}<newline><^END>
10 OUTPUT 717;":SENS1:OFFS:LOC:STOP 5E9"
20 OUTPUT 717;":SENS1:OFFS:LOC:STOP?"
30 ENTER 717;A