Property (Read-Write)
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STARt = Value
Value = SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STARt
This command sets/gets a start value for the external signal source frequency setting, for the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Setting of a start value for the external signal source |
|
Data type |
Double precision floating point type (Double) |
|
Range |
0 to 1E12 |
|
Preset value |
0 |
|
Unit |
Hz (hertz) |
|
Resolution |
1 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Start As Double
SCPI.SENSe(1).OFFSet.LOCal.FREQuency.STARt = 100E6
Start = SCPI.SENSe(1).OFFSet.LOCal.FREQuency.STARt
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.DIVisor
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.MULTiplier
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.OFFSet
SCPI.SENSe(Ch).OFFSet.LOCal.FREQuency.STOP
Sweep Setup > Frequency Offset > External Source > Start
:SENSe{[1]-160}:OFFSet:LOCal[:FREQuency]:STARt <numeric>
:SENSe{[1]-160}:OFFSet:LOCal[:FREQuency]:STARt?
{numeric}<newline><^END>
10 OUTPUT 717;":SENS1:OFFS:LOC:STAR 5E9"
20 OUTPUT 717;":SENS1:OFFS:LOC:STAR?"
30 ENTER 717;A