Command/Query
:CALCulate:EYE:INPut:DRATe <numeric>
:CALCulate:EYE:INPut:DRATe?
This command sets the bit rate for the simulated eye function.
|
Description |
Bit Rate |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
- |
|
Preset Value |
1G |
|
Unit |
bits/sec |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":CALC:EYE:INP:DRAT 1.1e9"
20 OUTPUT 717;":CALC:EYE:INP:DRAT?"
30 ENTER 717;A
:CALCulate:EYE:INPut:RTIMe:DATA
:CALCulate:EYE:INPut:RTIMe:THReshold
Eye/Mask > Data Rate (Under Bit Pattern)