:DISPlay:EYE:Y:SCALe:MANual

Type

Command Only

Syntax

:DISPlay:EYE:Y:SCALe:MANual

Description

This command changes the eye diagram scaling to manual mode. This command should be executed before the :DISPlay:EYE:Y:SCALe:PDIVision or :DISPlay:EYE:Y:SCALe:RLEVel commands are sent.

Examples

10 OUTPUT 717;":DISP:EYE:Y:SCAL:MAN"

Related Commands

:DISPlay:EYE:Y:SCALe:PDIVision

:DISPlay:EYE:Y:SCALe:RLEVel

Equivalent GUI

Eye/Mask > Scale/Mask > Manual radio button