Command/Query
:DISPlay:EYE:Y:SCALe:PDIVision <numeric>
:DISPlay:EYE:Y:SCALe:PDIVision?
This command sets value of y-axis scale per division for eye diagram. The scale mode should be set at manual by the :DISPlay:EYE:Y:SCALe:MANual before this command is executed.
|
Description |
Value of eye diagram y-axis scale per division |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
1E-18 to 5 |
|
Preset Value |
200m |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":DISP:EYE:Y:SCAL:MAN"
20 OUTPUT 717;":DISP:EYE:Y:SCAL:PDIV 300E-03"
30 OUTPUT 717;":DISP:EYE:Y:SCAL:PDIV?"
40 ENTER 717;A$
Eye/Mask > Scale/Mask > Manual radio button > Scale / Div