Command/Query
:DISPlay:EYE:Y:SCALe:RLEVel <numeric>
:DISPlay:EYE:Y:SCALe:RLEVel?
This command sets value of eye diagram y-axis reference line. The scale mode should be set at manual by the :DISPlay:EYE:Y:SCALe:MANual before this command is executed.
|
Description |
Value of eye diagram y-axis reference line |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
-5 to 5 |
|
Preset Value |
0 |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":DISP:EYE:Y:SCAL:MAN"
20 OUTPUT 717;":DISP:EYE:Y:SCAL:RLEV 0.01"
30 OUTPUT 717;":DISP:EYE:Y:SCAL:RLEV?"
40 ENTER 717;A
:DISPlay:EYE:Y:SCALe:PDIVision
Eye/Mask > Scale/Mask > Manual radio button > Offset