Command Only
:MMEMory:LOAD:EYE:MASK <string>
This command loads eye-mask file. The format of eye mask file should be the same as ones of Infiniium DCA (86100C). The extension of file should be .msk. The MASK pattern editing is not available through the command.
|
Description |
File name of eye mask (.msk) |
|
Data Type |
Character string type (String) |
|
Range |
- |
|
Preset Value |
- |
|
Unit |
- |
|
Resolution |
- |
See the example in :CALCulate:EYE:MASK:STATe
Eye Mask > Mask Pattern (under Eye Control) > File Tab > Load