Query only
:SENSe:SPURious:AVOid:STATe?
This command queries the avoid spurious state. This command is used only with Hot TDR mode.
This command is ON when :SENS:SPURious:AVOid:IMMediate command succeeds.
This command is OFF when :SENS:SPURious:AVOid:IMMediate command fails to find spurious.
|
Description |
Status of avoid spurious |
|
Data Type |
Boolean type (Boolean) |
|
Range |
1 (ON) or 0 (OFF) |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
{1|0} <newline><^END>
10 OUTPUT 717;":SENS:SPUR:AVO:STAT?"
:SENSe:SPURious:AVOid:IMMediate
Setup> Avoid Spurious (Under Hot TDR)
A green check mark is observed next to the Avoid Spurious button when Avoid Spurious state is successfully turned ON.