Query only
:SENSe:SPURious:STATe?
This command queries the Hot TDR mode status.
To turn ON Hot TDR mode, use :SENSe:SPURious:AVOid:IMMediate
To turn OFF Hot TDR mode, use :SYSTem:PRESet
|
Description |
Status of Hot TDR mode |
|
Data Type |
Boolean type (Boolean) |
|
Range |
1 (ON) or 0 (OFF) |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
{1|0}<newline><^END>
10 OUTPUT 717;":SENS:SPUR:STAT?"
:SENSe:SPURious:AVOid:IMMediate
"TDR ?" is indicated at the channel window. The blue SVC indicator is also turned ON.