Command/Query
:SENSe:SPURious:INPut:DRATe <numeric>
:SENSe:SPURious:INPut:DRATe?
This command sets the value of input bit rate for avoid spurious.
|
Description |
Value of input bit rate |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
1.21E6 to 16E9 |
|
Preset Value |
1E9 |
|
Unit |
bps |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":SENS:SPUR:INP:DRAT 1.5E9"
20 OUTPUT 717;":SENS:SPUR:INP:DRAT?"
30 ENTER 717;A
:SENSe:SPURious:AVOid:IMMediate
Setup> Data Rate (Under Hot TDR)