Property (Read-Write)
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.REFerence = Value
Value = SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.REFerence
This command turns sets/gets the reference receiver to be used in receiver leveling for the selected channel (Ch) and port (Pt).
|
Parameter |
Status |
|
Description |
Sets/gets the reference receiver for leveling sweep |
|
Data type |
Character string type (String) |
|
Range |
A|B|R1|R2 |
|
Preset value |
R1 |
Dim ref As String
ref = "A"
SCPI.SOURce(1).POWer.PORT(1).ALC.MODE.RECeiver.REFerence = ref
ref= SCPI.SOURce(1).POWer.PORT(1).ALC.MODE.RECeiver.REFerence
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.STATe
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.OFFSet
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.TOLerance
SCPI.SOURce(Ch).POWer.PORT(Pt).ALC.MODE.RECeiver.ITERation
Sweep Setup > Power > Receiver Leveling > Port 1|Port 2 > Receiver > A|B|R1|R2
:SOURce{[1]-160}:POWer:PORT{[1]|2}:ALC:MODE:RECeiver:REFerence {A|B|R1|R2}
:SOURce{[1]-160}:POWer:PORT{[1]|2}:ALC:MODE:RECeiver:REFerence?
{A|B|R1|R2}<newline><^END>
10 OUTPUT 717;":SOUR1:POW:PORT1:ALC:MODE:REC:REF A"
20 OUTPUT 717;":SOUR1:POW:PORT1:ALC:MODE:REC:REF?"
30 ENTER 717;A$