Other topics about Setting Control Functions
This section describes how to set the interface necessary to use the GPIB (General Purpose Interface Bus) of the E5072C.
When controlling the E5072A using GPIB commands from the external controller connected to the GPIB connector, you need to set the talker/listener GPIB address of the E5072A.
Follow these steps to make this setting:
Press System.
Press Misc Setup > GPIB Setup> Talker/Listener Address.
Enter the address using the ENTRY block keys on the front panel.
When controlling an external device from the E5072A, connect the USB port of the E5072A and the GPIB port of the external device through the USB/GPIB interface.
Do not connect two or more USB/GPIB interfaces.
Before following the steps mentioned below, ensure that the drive for 82357B is installed.
Follow these steps to set the USB/GPIB interface:
Connect the USB port of the E5072A to the USB/GPIB interface.
Select No, not this time, then click Next.

Select Install the software automatically (Recommended), then click Next.

Click Finish.

The Found New Hardware Wizard appears again. Repeat the step 2 to 4 again.

Select When a new 82357 is plugged in, then click OK.

Select "When a new <USB device> is plugged in." or "Never show this dialog" instead of "Each time a USB devices is plugged in".
If you need to check/change the setting of the USB/GPIB interface after connecting the USB/GPIB interface, follow these steps:
Press System, then click Misc Setup > GPIB Setup > System Controller Configuration.
The Keysight Connection Expert appears. (You can also execute Keysight Connection Expert from Task bar or Start menu in Windows.)

Select USB/GPIB (GPIBx).
Click Change Propetries...
Change the setting of USB/GPIB interface.
It is required to connect the USB/GPIB Interface to "GPIB0" as VISA Interface ID, in order to control:
Power Meter for the Power Calibration
External Signal Source for the Frequency Offset