Executing the Back-end Application in VNA

Other topics about Measurement Wizard Assistant

Overview

The back-end application of the MWA is a program running on the VNA. The back-end application reads a spec sheet (.mwa) created by the MWA front-end application, and automatically sets up all the measurement parameters on the VNA. Based on the information included in the spec sheet,the back-end application sets up the VNA multiport test set, or the external peripherals,and executes measurement procedure the detailed analysis report of the results.

Starting MWA (Back-end Application)

A method for starting the back-end application of the MWA on the VNA is explained below.

  1. Press Macro > Macro 1 > MWA.

Description of Windows

The back-end application of the MWA has the following windows:

  1. Main Window

  2. Spec Sheet Setting Window

  3. Connection Information Window

  4. Calibration Wizard Window

  5. All Spec Sheets Measurement Window

  6. Measurement by Spec Sheet Window

  7. Results Verification by Mode Window

1. Main Window

This is the first window displayed after startup.

In this window, the following buttons can be selected for enabling functionality available in the back-end application

Main Window

Displays Spec Sheet Setting Window.

Clears group files that have been already read in the Spec Sheet Setting Window.

Displays Calibration Wizard Window (1/2)for automatic calibration procedure.

Saves a status file on the VNA. As a status file is automatically saved in the VNA when saving a group file or the necessary calibration is completed in the Calibration Wizard Window, it is not necessary to press this button if the setting on the VNA is not changed.

Displays Connection Information Window for verifying the connectivity of the network analyzer, the multiport test set, and the DUT.

Displays All Spec Sheet Measurement Window for launching measurement procedure.

Minimizes the window of the back-end application. This function provides easy access to the display of the VNA for changing parameters after recalling a spec sheet.

The recalled group files with the list of spec sheets are displayed in the Main Window after the setup in the Spec Sheet Setting Window (link inserted). The name of spec sheets, the number of group files, and the allocated channel number of the VNA are included. The option button for each group file can be enabled for selecting the active group file used in the measurement.

If multiple spec sheets are bundled in a group file, the option button of the first sheet can be enabled for the group file (It is not necessary to select the other spec sheets).

The group with the circle mark (● ) on the option button is the current active group. The calibration performed in the Calibration Wizard Window and the measurement is effective for this active group. The state file is saved by the Save State button (Main Window ) for the active group file as well.

2. Spec Sheet Setting Window

In this window, spec including all the parameters for the setup on the VNA are recalled. The multiple spec sheets are bundled into one group and handled as a group file (.ssg) in the following procedure of the back-end application. Up to 10 different spec sheets can be added in one group file.

 Spec Sheet Setting Window

Recalls a saved group file (.ssg).

Creates a new group file (.ssg).

Displays the file selection dialog for status files of the group.

Adds a spec sheet (.mwa) under the group file. The default name of the group file is named after the recalled spec sheet.

Clears all the spec sheets that have been already recalled in the window.

Reflects all the settings on the VNA according to the recalled spec sheets and returns to the Main Window. The state file for the group is saved automatically.

Discards the settings and returns to Main Window.

3. Connection Information Window

This window is displayed when Connection Information in the Main Window is selected.

Using the label names defined in the front-end application, this window shows information on the connection between the VNA, the multiport test set(s),and the DUT.

Connection Information Window

Closes the window and returns to the Main Window.

 

4. Calibration Wizard Window

This window is displayed when Cal Wizard in the Main Window is selected.

The wizard provides the necessary steps of the calibration procedure with the VNA and the multiport test set in accordance with the contents of recalled spec sheets.

Calibration Wizard Window (1/2)

Displays the calibration types that can be performed with the calibration wizard.
 

These include Mechanical Cal Kit (calibration with the mechanical calibration kit), 4-Port ECal (calibration with the 4-port ECal module), Source Power Cal and Receiver Power Cal (Receiver calibration).

Displays the list of mechanical calibration kits available on the VNA for the calibration. This can be selected when Mechanical Cal Kit is selected as the calibration type.

Displays the list of characteristics registered in the ECal modules. User-defined characteristics of the ECal module (User 1 to 5) can be selected for calibration with different types of connectors.

Sets the averaging number for measurements during calibration. This averaging number is used only during calibration and returns to the original number registered in the VNA when calibration is completed.

Calibration Wizard Window (2/2): mechanical calibration kit selected

Calibration Wizard Window (2/2): 4-port ECal selected

Performs calibration measurement with the displayed connection.

Goes back to the previous step in the Calibration Wizard.

Goes to the next step in the Calibration Wizard after the calibration measurement is completed.

Aborts the Calibration Wizard and returns to the Main Window.

Performs the correction of error coefficients on every necessary port then returns to Main Window.

5. Measurement Window

All Spec Sheets Measurement Window

This window is displayed after the setup in the Lot Input Window when the Measurement button in the Main window is selected.

Spec sheets and summaries of their measurement results are listed in this window. To check the results by spec sheet, select each spec sheet in this window and press Manual Trigger.

All Spec Sheet Measurement Window

Displays Measurement by Spec Sheet Window.

The spec sheet button with the black triangle icon to its left indicates the next sheet to be measured.

Only the spec sheet with a checked mark is measured.

Rescale the Measurement Window of the back-end application with the half size of the screen. The window is located at the bottom half of the screen and the measurement results of the VNA is displayed in the top half. See the Measurement Window in half mode.

Minimizes the Measurement Window. See the minimized window.

Makes an immediate measurements with manual trigger on the checked spec sheets in the window. (The black triangle icon is displayed to the left of the Spec Sheet button.)

Skip the measurement of the spec sheet with a black triangle icon on the left.

Ends measurement in the current window, saves the results, and displays All Spec Sheet Measurement Window with a new lot name.

Ends measurement in the current window and returns to the Main Window. The measurement results are saved in the designated directory of the VNA.

Measurement by Spec Sheet Window

This window is displayed by selecting one of the buttons for the spec sheets that are listed in the All Spec Sheets Measurement Window.

This window shows a list of the measurement modes in the selected spec sheet. To make measurements while checking measurement results in different measurement modes, press Manual Trigger in this window.

 Measurement by Spec Sheet Window

Makes an immediate measurement with manual trigger on the checked spec sheets in the All Spec Sheets Measurement window.(The same function on the Manual Trigger button in the All Spec Sheets Measurement Window).

Returns to the All Spec Sheet Measurement window.

Results Verification by Mode Window

This window is displayed by selecting one of the buttons for the measurement modes listed in the Measurement by Spec Sheet Window.

This window shows a list of measurement results for the measurement paths specified in the selected measurement mode.

Results Verification by Mode Window

Path: The label name of a measurement path that is defined in the "Spec Sheet" in the front-end application.

 

Spec Min/Max: The maximum and minimum limit values of the DUT specification for the measurement paths. These values are entered in the "Spec Sheet" in the front-end application.

 

Worst Value: The limit test by the back-end application is performed for each measurement point and the worst value of the DUT is displayed in the measurement result. The worst value is defined as the farthest value from the average of the maximum and minimum limit values, which corresponds to the typical measured data of the DUT.

 

Pass/Fail: Indicates the result of the limit test for all data in the measured path.

 

Rank: The rank value of each measurement path (specified in the Spec Sheet sheet in the front-end application). The result of the limit test can be prioritized and sorted in all the measurement paths with the fail. The back-end application outputs the minimum rank value among the failed measurement paths. For example, by assigning the smallest rank value for a specific measurement path, you can identify the worst performance of the DUT with the output of the rank value after the measurement.

If the result of the limit test gives pass for all the measurement paths, the output rank value is "0".

The definition of the pass/fail result of the measurement can be ranged by the Max Fail Rank specified in the Lot Input Window of the back-end application. When the rank value is greater than the max fail rank value, the failed result of the limit test is treated as pass, and the corresponding rank values for measurement paths are outputted in the result. The following table shows an example of the output rank values, when (the Max Fail Rank is set to 200).

Rank value for path

Pass/Fail

Rank to be output

1 - 200

Fail

1 - 200

201 - 255

Pass

201 - 255

 

For the measurement value, Worst Value, and Pass/Fail judgment, refer to step10 of the Setting Up Measurement Parameters in Each Mode.

Returns to Measurement by Spec Sheet Window.

 

6. Other Windows

Measurement Window in Half mode: This window is shown when half in the All Spec Sheets Measurement Window is pressed.

You can use this window when you want to use the MWA while watching the measurement result displayed in the screen of the VNA. In this window, only a failed measurement path is displayed and you can check the corresponding channel and trace for further investigation of the result.

If the measurement paths cannot be displayed in one screen, the <<Prev button and the Next>> button become effective.

If you check the Disp enable check box, Display Update function of VNA is activated for drawing the image on the screen. It is recommended to disable this function and save time for updating the display when the fast testing speed is really required.

Measurement Window in Half Mode

Lot Input Window

The lot input window is used for the setup of the measurement.  For more information, refer to the Measurement Procedure (All Spec Sheets Measurement Window).

Lot Input Window

 

Selecting and Clearing Spec Sheets

The procedure described below is for selecting or clearing spec sheets in the Main Window or in the Spec Sheet Setting Window.

Selecting Spec sheets

  1. Press Add Spec Sheet Group in the Main Window to display the Spec Sheet Setting Window.

  2. To create a new group, press Create New Group... in the window, type the name of the new group in the file dialog, and press Save.

    To recall an existing group, press Read Group File... in the window, select the group file in the file dialog and press Open.

    The full path name of the group file entered or selected is displayed in the window

  1. To specify the state file to be associated with the group, press Browse... in the State File frame, select the state file to recall and press Open.

    The full path name of the selected state file is displayed in the window.

  2. Press Add Spec Sheets... in the window. Select the spec sheet to use in measurements and press Open.

The name of the selected spec sheet and allocated channel numbers in VNA will be displayed in the window.

  1. After selecting all the necessary spec sheets, press OK to return to the Main Window. The name of the spec sheet and the allocated channel information will be displayed in the Main Window.

    All the functions in the Main Window become available after the spec sheet is imported in the back-end application.

  2. When no spec sheet is imported or all the spec sheets are cleared by Clear All Groups, the buttons in the Main Window are Disabled and the related their functions become unavailable.

Clearing group files

  1. Select Clear All Groups in the Main Window after setting up the group file in the Spec Sheet Setting Window.

  2. All the group files are cleared and all the buttons in the Main Window become Disabled and the related functions become unavailable.

  3. It is not available to clear each group file individually.

 

Checking Connections

The procedure described below is for checking the connection between the measurement instruments and the DUT in the Connection Information Window.

  1. Select Connection Information in the Main Window after recalling a spec sheet.

  2. The Connection Information Window is displayed. Based on the information on the screen, connect the cables between the VNA, the multiport test set(s) and the DUT.

  3. After checking that the connection is correct, press Close to close the window and return to the Main Window.

 

Calibration Procedure

The procedure described below is for performing the calibration procedure by the Calibration Wizard Window of the back-end application.

  1. Select a group file to calibrate with the radio button in the Main Window.

  2. Select Cal Wizard in the Main Window.

  3. The calibration wizard starts up and the Calibration Wizard window (1/2) is displayed. From the list of types of calibration shown in the window, select the type of calibration to perform. The following options are available:
     

    Type of Calibration

    Description

    Mechanical Cal Kit

    Uses a calibration kit to perform calibration. For information on the selecting a calibration kit, refer to Step 4.

    4 Port ECal

    Uses 4-port ECal to perform calibration.

    Receiver Cal

    Performs Receiver calibration while making FOM measurements.

  1. If Mechanical Cal Kit is selected in Step 3, the list of calibration kits available for selection is displayed in the window. Select the appropriate calibration kit to use.
    If 4-port Ecal has been selected in Step 3, the list of user-defined characteristics of the ECal module is displayed in the window. Select the appropriate characteristics of the ECal module to use. Refer to User-characterized ECal for more detail.

Note: The information on displayed calibration kits has been imported from the VNA firmware. When the parameters of the calibration kit are changed in the VNA, corresponding information will be reflected in the back-end application as well.

  1. Enter the number of averaging during the calibration measurement into the Averaging Count input box. All the parameters on the calibration kit are selected, press Next for the next step in the calibration procedure.

  2. The Calibration Wizard Window (2/2) will be displayed. Both the ports of the VNA or the multiport test set and the calibration standards  used for the calibration are displayed. Connect the ports with the standard and press Measure. After the calibration measurement is completed, press Next > for the next step.

  3. Repeat Step 6 as many times as needed for all the calibration steps necessary for the selected spec sheets. After all the calibration measurement is completed, press Done and return to the Main Window. The Calibration data will be saved in the state file of the selected group file automatically.

  1. When performing calibration with ECal,the MWA back-end application shows "Execution error" if active channel is selected for trigger scope on the VNA firmware. Hence, select All Channels for the trigger scope.

Saving State File

The procedure for saving state files  in the Main Window is described below.

The State file for a group is automatically saved when you create a group file in the Spec Sheet Setting Window or you perform calibration in the Calibration Wizard Window. If parameters on the VNA are changed without using the functions of the back-end application, a state file should be saved manually in the Main Window.

  1. Press Save State in the Main Window.

  2. The State Files (.sta) of the current active groups are updated.

 

Measurement Procedure (All Spec Sheets Measurement Window)

The procedure described below is for making measurements by spec sheet in the All Spec Sheets Measurement Window.

  1. After the setup of spec sheets in the Spec Sheet Setting Window,  press Measurement in the Main Window. The lot Input Window is displayed.

  2. Enter the lot name of the DUT. Check optional functions in the measurement as necessary and press OK.

This option allows you to write measured values at the start and stop frequencies to a result file of the measurement. The back-end application automatically generates the result file for each spec sheet after the measurement. Refer to Measurement result by spec sheet.

This option allows you to reflect the correction on measured values specified in the “Spec Sheet” front-end application, refer to Step 9 in the Setting Measurement Parameters in Each Mode.

This option enables the Manual Trigger button in the All Spec Sheets Measurement Window and the Measurement by Spec Sheet Window. When this option is not checked, manual measurements using the Manual Trigger button cannot be made.

This option allows you to overwrite or add the measurement result when a result output file already exists. When this option is checked, the existing file is overwritten.

This option sets the maximum rank value for the fail result in the limit test. For example, when "max fail rank" is set to 10, the result for measurement paths with ranks 1 through 10 treated as fail and 11 through 255 treated as pass. For more information, refer to rank in Measurement results display area.

When you press the OK button, the All Spec Sheet Setting Window is displayed.

  1. Press Skip to place the black triangle icon to the left of the desired spec sheet with which measurements are made.

  1. With the black triangle icon placed to the left of the spec sheet for use during measurement, press Manual Trigger to perform measurement.

To do the measurement for the selected measurement paths that have been checked in the "Spec Sheet” of the front-end application, check Selected Measurement and press Manual Trigger.

To make consecutive measurements using the displayed spec sheets, check the Continuous check box.

  1. When measurements for the spec sheets are completed, the measurement result (Pass or Fail) is displayed to the right of each spec sheet.

Note: To check measurement result for each spec sheet, press the button of the desired spec sheet to display the Measurement by Spec Sheet Window. For information on the Measurement by Spec Sheet Window, refer to Measurement Procedure (Measurement by Spec Sheet Window).

Measurement Procedure (Measurement by Spec Sheet Window)

The procedure described below is for selecting one of the spec sheets in the measurement window, and making detailed measurement in the Measurement by Spec Sheet Window for each measurement mode included in the spec sheet.

  1. In the All Spec Sheets Measurement Window, press the button of the desired spec sheet to display the Measurement by Spec Sheets Window for the spec sheet.

  2. Press Manual Trigger to launch the measurement for each mode in the selected spec sheet.

To do the measurement for the selected measurement paths that have been checked in the Spec Sheet” sheet of the front-end application, check the box for Selected Measurement and press Manual Trigger.

To make consecutive measurements with continuous sweep for all the measurement modes, check the Continuous check box.

  1. When measurements are completed, the letter "P" (for Pass) or "F" (for Fail), is shown to the right of the measurement mode. Press Close, to return to the All Spec Sheets Measurement Window.

Note: To check detailed measurement results for each measurement mode, press the button for the desired measurement mode to display the Results Verification by Mode Window. For information on the Results Verification by Mode Window, refer to Measurement Procedure (Results Verification by Mode Window).

Measurement Procedure (Results Verification by Mode Window)

The procedure described below is for selecting one of the measurement modes and checking results by measurement path in the Results Verification by Mode Window.

  1. To display the Results Verification by Measurement Mode Window, press the button of the desired measurement mode in the Measurement by Spec Sheet Window.

  2. Measurement results for each measurement path are listed in the Results Verification by Measurement Mode Window. For more details in the listed parameters, refer to measurement results display area in the Results Verification by Mode Window.

Created Results File

This section describes measurement result files that are created at the end of a measurement.

  1. Measurement result summary by lot

This file is created at the end of a measurement or when the name of a lot is changed by selecting New Measurement in the All Spec Sheets Measurement Window. It is created in csv format and saved automatically in the VNA.

The content of the created file is shown in Measurement result summary by lot.

Measurement result summary by lot

The first line is the header of a file and the second line or below contains the measurement result for each spec sheet. The following parameters are included in the result:

  1. Measurement result by spec sheet

The file of measurement result is created separately for each spec sheet. Each file is created in csv format ("Lot name"-"spec sheet name".csv) and saved automatically in the same folder as each spec sheet (.mwa) of VNA. The content of the created file is changed depending on the selection of the “output start/stop value” check box in the Lot Input Window.

The content of the created file is shown in Measurement result by spec sheet.

Files of measurement results by spec sheet (start/stop value: ON)

"Index","Rank","Mode1-Path1",,,"Mode1-Path2",,,"[GPIB**Address] GPIB Command, ... ,"ModeX-PathY",,

,,"Start","Stop","Worst", ... ,"Meas", ... ,"Start","Stop","Worst", ...

1,Output Rank,Start_Value,Stop_Value,Worst_Value, ... ,GPIB_Response Value, ... ,Start_Value,Stop_Value,Worst_value, ...

2,Output Rank,Start_Value,Stop_Value,Worst_Value, ... ,GPIB_Response Value, ... ,Start_Value,Stop_Value,Worst_Value, ...

...

N,rOutput Rank,Start_Value,Stop_Value,Worst_Value, ... ,GPIB_Response Value, ... ,Start_Value,Stop_Value,Worst_Value, ...

The first and second lines are the header of a file, and the third line or below contains all the measurement result for the spec sheet. The following parameters are included in the file:

All the measurement values of a single DUT are summarized in one line. When multiple measurements are performed for a spec sheet, the multiple measurement results in additional lines are included in the file.

As the measurement value at the start/stop frequency is not available for the measurement type such as “mean” or “ripple”, no data is recorded in the start/stop values for the path.

Note: Even when the measurement for a spec sheet is skipped by the Skip button in the All Spec Sheets Measurement Window, the result is recorded in the file as well. However, the output rank is fixed to -1 and no measured values are recorded for the start/stop or worst values.

When "Output Start/Stop value" is disabled by the Lot Input Window in advance of the measurement, the contents of the output is shown below:

Measurement result by spec sheet (start/stop value: OFF)

"Index","Rank","Mode1-Path1",,,"Mode1-Path2",,,"[GPIB**Address]GPIB Command", ... ,"ModeX-PathY",,

1,Output Rank,Worst_value, ... ,GPIB Response Value, ... ,Worst_Value, ...

2,Output Rank,Worst_value, ... ,GPIB Response Value, ... ,Worst_Value, ...

...

N,Output Rank,Worst_value, ... ,GPIB Response Value, ... ,Worst_Value, ...

Controlling the Back-End Application From An External PC

The procedure for controlling the back-end application from an external PC is described below.

  1. Send the following commands to the VNA via GPIB.

DISP:WIND1:TITL:DATA (Command Parameter)

The following command parameters are available with the MWA.

Command Parameter

cmd_para function

Argument 1

Argument 2

Window that accepts the command

cmd_read

Group file name (.ssg) or spec sheet name (.mwa)

 

Main Window

cmd_clear

-

 

Main Window

cmd_begin

Lot name

Parameters in the Lot Input Window. For more details, refer to Measurement Procedure (All Spec Sheets Measurement Window)

Main Window, Measurement Window

cmd_initiate

-

 

Measurement Window

cmd_skip

-

 

Measurement Window

cmd_settings

Correction values, Manual measurement

 

Measurement Window

cmd_end

-

 

Measurement Window

Each of the cmd_para functions as follows.

cmd_para functions

Description

Corresponding buttons

cmd_read

Reads the group file or spec sheets specified by the argument 1. If you send this command when no file exists or no more files can be read, an error occurs.

To specify multiple spec sheets, specify spec sheets separated with commas when assigning an argument 1 in Step 2.

Main Window

Add Spec Sheet Group

cmd_clear

Clears all spec sheets that are currently read.

Main Window

Clear All Groups

cmd_begin

Displays the All Spec Sheets Measurement Window, specifying a lot name of the DUT by using argument 1.

Argument 2 specifies the option for the measurement (the same setup in the Lot Input Window). For more details, refer to Measurement Procedure (All Spec Sheets Measurement Window). For each option, refer to that page.

  • Output Start/Stop Values

The same as Start/Stop values. Specifies 0 (OFF) or 1 (ON).

  • Correction values

The same as Correction (Limit Test). Specifies 0 (OFF) or 1 (ON).

  • Manual Measurement

The same as enable Manual Measurement. Specifies 0 (OFF) or 1 (ON).

  • Overwrite Output File

The same as Overwrite Output File. Specifies 0 (OFF) or 1 (ON).

  • Max Fail Rank

The same as max fail rank (1-255). Specifies the value from 1 to 255.

If you send this command when each measurement window is displayed, a summary of the results is generated to a file, the current measurement is closed, and the All Spec Sheets Measurement window opens with a new lot name.

Main Window

Measurement

All Spec Sheets Measurement Window

New Measurement

cmd_initiate

Initiates measurement immediately.

All Spec Sheets Measurement Window

Manual Trigger

Measurement by Spec Sheet Window

Manual Trigger

cmd_skip

Skips the measurement of the next spec sheet.

All Spec Sheets Measurement Window

Skip

cmd_settings

Changes the option of correction values and manual measurement during the measurement. For correction values and manual measurement, refer to the descriptions of cmd_begin.

None

cmd_end

Outputs summary of the results and returns to the Main Window.

All Spec Sheets Measurement Window

End Measurement

  1. If it is necessary to set the argument for a command, the following command is required before sending the command in Step 1. If each argument has several items, set all the parameters separated by a comma (,).

DISP:WIND2:TITL:DATA parameter

DISP:WIND3:TITL:DATA parameter

For example, to start new measurement using the lot name "lot_gsm001," send the following command. In the following example, the output start/stop value and overwrite output file are turned ON and the max fail rank is set to 100.

10 output 717;"DISP:WIND2:TITL:DATA lot_gsm001"
20 output 717;"DISP:WIND3:TITL:DATA 1,0,0,1,100"
30 output 717;"DISP:WIND1:TITL:DATA cmd_begin"

Note: If you send a command with incorrect arguments, the command is not executed.

When the command process finishes, the return value of DISP:WIND1:TITL:DATA? becomes "cmd_done" If you want to wait for the command process to finish, confirm this by whether the returned value of DISP:WIND1:TITL:DATA? is "cmd_done"

Operation of Handler I/O Port by MWA

A list of pins of the handler I/O operated by the MWA is shown below. The signal notations in the parentheses correspond to those of the VNA. For details, refer to I/O Signal Pin Layout and Description.

Pin number

Signal Name in MWA (signal name in normal mode)

Direction of signal

Description

2

/INPUT

(/INPUT1)

Input

When a negative pulse is applied to this pin, the level of the signal /OUTPUT1 becomes Low.

3

/INIT (/OUTPUT1)

Output

When a negative pulse is applied to pin 2, the level of /OUTPUT1 becomes Low.

The back-end application monitors /OUTPUT1 and when it turns Low, starts measurement. /OUTPUT1 returns to High at the start of a measurement.

In addition, the "CONT:HAND:OUTP1:DATA 1" command can be used to set the signal level to Low or High.

5

/RANK A0

(/PORT A0)

Output

Outputs the minimum rank value for the measurement. The output rank is the 8-bit value (0-255) with A0 as LSB and A7 as MSB.

/PORT A0 is bit 0 of the output rank.

6

/RANK A1

(/PORT A1)

Output

Bit 1 of the output rank.

7

/RANK A2

(/PORT A2)

Output

Bit 2 of the output rank.

8

/RANK A3

(/PORT A3)

Output

Bit 3 of the output rank.

9

/RANK A4

(/PORT A4)

Output

Bit 4 of the output rank.

10

/RANK A5

(/PORT A5)

Output

Bit 5 of the output rank.

11

/RANK A6

(/PORT A6)

Output

Bit 6 of the output rank.

12

/RANK A7

(/PORT A7)

Output

Bit 7 of the output rank.

13

/FAIL

(/PORT B0)

Output

If the limit test fails, /PORT B0 becomes enabled (Low level). If the output rank value (/PORT A0 - /PORT A7)is 0 (which corresponds to the pass for all measurements), /PORT B0 becomes disabled (High level).

This signal transits after the output /RANK (/PORT A0 to A7) transition, but transits almost the same timing of the /INDEX (/PORT B4) transition. Be sure to check /FAIL with some delay after /INDEX transition.

17

/INDEX

(/PORT B4)

Output

A signal that indicates the end of measurement.

The signal transits after the output rank (/PORT A0 - /PORT A7) transition.

The back-end application sets /PORT B4 back to inactive (High level) at the start of measurement.

19

/INDEX_SUB

(/PORT B5)

Output

A reserved signal pin with the same function as /PORT B4. Either pin can be used.

22

/SKIP

(/PORT C0)

Input/Output

This is a skip signal.

If /PORT C0 is enabled (Low level) before measurement, the measurement is not performed and the status shifts to the mode of waiting for the next measurement.

Error messages in the Back-End Application

While working with MWA, an error message may appear due to improper VNA settings. This section explain the various error messages and the method to avoid these errors.

 

Error Message

Description

Channel Max

This error message appears if the total number channels required for a spec sheet (.mwa) is more than the number of channels set in the VNA.

Note: This error can be avoided by increasing the maximum number of channels in VNA.

Configuration and test set are mismatched.

This error message appears if the configuration of the test set specified in a spec sheet (.mwa) generated by the Front-End Application is different from the test set that is being connected to the VNA.

This error can be avoided by changing the configuration of the Multiport Test Set sheet in the Front-End Application. For more info, refer to Selecting Test Set.

 

This error may appear if:

  • The configuration in a spec sheet is for the E5091A (E5092A), but the E5092A (E5091A) is connected to the VNA.

  • The configuration in a spec sheet is with the multiport test set (E5091A or E5092A), but no test set is connected to the VNA.

  • The configuration in a spec sheet is "None" (no test set), but the test set is connected to the VNA.

GPIB Error

This error message appears if the GPIB address of peripherals connected to the VNA is different from what you specified in the GPIB sheet of the front-end application.

Invalid number of point

This error message appears if the maximum number of points required for a spec sheet (.mwa) is more than the number of points set in the VNA.

Note: This error can be avoided by increasing the maximum number of channels in VNA.

Invalid Trace

This error message appears if the maximum number of traces required for a spec sheet (.mwa) is more than the number of traces set in the VNA.

Note: This error can be avoided by increasing the maximum number of channels in VNA.