Only the Main, Compression Levels, and Leveling & Offsets Power commands corresponding to the Gain Compressions and Gain Compression Converters measurement classes are documented here. The Attenuators commands are identical to the Attenuator commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtab on the graphic below.
Click here to view links to Power commands for all Measurement Classes.