Initiates a Power Saturation marker search and reads the results.
These commands are Superseded by the CALCulate:MEASure:MARKer:PSAT commands.
|
CALCulate:MARKer:PSATuration COMPression | MAXimum? | SATuration? GAIN? | LINear? | MAXimum? PIN? | MAXimum? POUT? | MAXimum? |
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Turns on and sets markers 1, 2, and 3 to calculate various Power Saturation parameters. The <num> parameter sets and reads the back-off value for a Power Saturation marker search. To turn off the Power Saturation markers, either turn them off individually or turn them All Off. To search a User Range with the PSAT search, first activate marker 1 and set the desired User Range. Then send the CALC:MARK:PSAT:BACK command. The user range used with the PSAT search only applies to marker 1 searching for the linear gain value. The other markers may fall outside the user range. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<num> |
Backoff value. Choose any number between :-500 and 500 |
|
Examples |
CALC:MARK:PSAT:BACK 3 |
|
Query Syntax |
CALCulate<cnum>:MARKer:PSATuration:BACKoff? |
|
Return Type |
Numeric |
|
0 |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the compression maximum value from a PSAT marker search. Comp Max = Gain Max - Gain Linear Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:COMP:MAX? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the compression saturation value from a PSAT marker search. Comp Sat = Gain Sat - Gain Linear Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:COMP:SAT? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the saturation gain value from a PSAT marker search. Gain Sat = Psat Out - Psat In Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:GAIN? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the linear gain value from a PSAT marker search. Gain Linear = Marker 1 - Y-axis value MINUS X-axis value. Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:GAIN:LIN? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the maximum gain value from a PSAT marker search. Gain Max = PMax Out - PMax In Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:GAIN:MAX? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the power saturation input value from a PSAT marker search. Psat In = Marker 2 X-axis value Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:PIN? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the maximum input power from a PSAT marker search. PMax In = Marker 3 X-axis value Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:PIN:MAX? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the back-off output power from a PSAT marker search. PSat Out = Marker 2 Y-axis value Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:POUT? |
|
Not applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Reads the back-off output power from a PSAT marker search. PMaxOut = Marker 3 Y-axis value Use CALC:MARK:PSAT:BACK to initiate a PSAT search. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MARK:PSAT:POUT:MAX? |
|
Not applicable |
|