Learn about Receiver Attenuation
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets the attenuation level for the specified receiver. Note: Attenuation cannot be set with Sweep Type set to Power |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<recvr> |
Receiver to get attenuation. Choose from:
Receiver attenuation can NOT be set using logical receiver notation. |
|
<num> |
Attenuation value in dB. To determine how many receiver attenuators, the maximum receiver attenuation, and attenuation step size, for a VNA model, see VNA Models and Options. If a number other than these is entered, the analyzer will select the next lower valid value. For example, if 19 is entered for the E8361A/C, then 10 dB attenuation will be selected. |
|
Examples |
SENS:POW:ATT AREC,10 |
|
Query Syntax |
SENSe<cnum>:POWer:ATTenuator? <rec> |
|
Return Type |
Numeric |
|
0 |
|