Contains the settings to create and control Dynamic Uncertainty for S-Parameters (Opt. S93015A).
|
Setup Options |
|
|
|
|
|
Noise Characterization |
|
|
Clear noise data on specified port |
|
|
Clear noise data on all ports |
|
|
Copy noise from a port to all ports |
|
|
Start Noise char |
|
|
List cables |
|
|
Assign Cable to all ports |
|
|
Assign Cable to specified port |
|
|
Reset repeatability |
|
|
Start Cable char |
|
|
Load workspace |
|
|
Save workspace |
|
|
Enable a Guided Cal to include Uncertainties |
|
|
Checkbox on Guided Cal Select Ports page |
|
![]() |
CALC:MEAS:UNC:DISP:TYPE |
|
CALC:MEAS:UNC:DISP:CFAC |
|
|
CALC:MEAS:UNC:MOD:NOIS |
|
|
CALC:MEAS:UNC:MODE:CABL:REP |
|
|
CALC:MEAS:UNC:MOD:ETER |
|
|
Apply to all traces |
None |
|
Add Trace |
None |
|
Save uncertainty data |
CALC:MEAS:UNC:SAVE |
Calibrations can be performed for ONLY ONE channel at a time.
Putting Error Term data into Uncertainty Cal Sets using remote commands is NOT supported.
Trace Commands for Dynamic Uncertainty
Learn more about Dynamic Uncertainty
Example Program
|
Applicable Models: N522xB, N523xB, N524xB (Read-only) Returns a comma-delimited list of names of cables that are defined in the Uncertainty Manager application. |
|
|
Parameters |
None |
|
Examples |
SYST:UNC:CABL:CAT? |
|
Return Type |
Comma-delimited string |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Resets (clears) the characterized repeatability data associated with the specified cable. |
|
|
Parameters |
|
|
<cableName> |
String. Name of the cable for which data is to be reset. |
|
Examples |
SYST:UNC:CABL:REP:RES "MyCable" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Sets the name of the cable to be associated with all the ports currently enabled on the VNA |
|
|
Parameters |
|
|
<cableName> |
String. Name of the cable. |
|
Examples |
SYST:UNC:PORT:CABL:ALL "MyCable" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-Read) Sets and returns the name of the cable to be associated with the specified port number on the VNA |
|
|
Parameters |
|
|
<pNum> |
VNA port number. |
|
<cableName> |
String. Name of the cable. |
|
Examples |
SYST:UNC:PORT3:CABL "MyCable" |
|
Query Syntax |
SYSTem:UNCertainty:PORT<pNum>:CABLe[:SELect]? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Copies the characterized noise data associated with the specified port, to all the other ports |
|
|
Parameters |
|
|
<pNum> |
VNA port number for which noise data will be copied. |
|
Examples |
SYST:UNC:PORT:NOIS:ALL:COPY 2 |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Resets (clears) the characterized noise data for all currently enabled VNA ports. |
|
|
Parameters |
None |
|
Examples |
SYST:UNC:PORT:NOIS:ALL:RESet |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Resets (clears) the characterized noise data for the specified VNA port. |
|
|
Parameters |
None |
|
<pNum> |
VNA port number for which noise data will be reset. |
|
Examples |
SYST:UNC:PORT2:NOIS:RESet |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Loads an uncertainty ‘workspace’ (*.ml4) file into the Uncertainty Manager. |
|
|
Parameters |
None |
|
<filename> |
String. Full path, filename, and extension of the uncertainty workspace file, enclosed in quotes. |
|
Examples |
SYST:UNC:LOAD "C:\MyUncert.ml4" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-only) Saves the current uncertainty ‘workspace’ of the Uncertainty Manager to a (‘.ml4’) file. |
|
|
Parameters |
None |
|
<filename> |
String. Optional argument. Full path, filename, and extension of the uncertainty workspace file, enclosed in quotes. If filename is not specified, the current workspace is saved to the default workspace (*.ml4) file. |
|
Examples |
SYST:UNC:STORe "C:\MyUncert.ml4" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-Read) Sets and returns the maximum number of points (“decimation value”) for which uncertainties are to be computed for subsequent calibrations that are performed using Dynamic Uncertainty for S-Parameters. |
|
|
Parameters |
|
|
<num> |
Max number of points. Specify an integer between 0 and 501. |
|
Examples |
SYST:UNC:POIN:MAX 201 |
|
Query Syntax |
SYSTem:UNCertainty:POINts:MAXimum? |
|
Return Type |
Numeric |
|
500 |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-Read) Sets and returns the ON/OFF state of allowing noise data to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty for S-Parameters. Noise data must also be present for the ports at the time the calibration is performed. |
|
|
Parameters |
|
|
<bool> |
Enable ON/OFF state. Choose from: ON or 1 - Noise uncertainty ON. OFF or 0 - Noise uncertainty OFF. |
|
Examples |
SYST:UNC:ETER:NOIS:ENAB ON |
|
Query Syntax |
SYSTem:UNCertainty:ETERm:NOISe:ENABle? |
|
Return Type |
Boolean |
|
ON |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-Read) Sets and returns the ON/OFF state of allowing cable repeatability data to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty for S-Parameters. Repeatability data must also be present for the ports at the time the calibration is performed. |
|
|
Parameters |
|
|
<bool> |
Enable ON/OFF state. Choose from: ON or 1 - Cable repeatability uncertainty ON. OFF or 0 - Cable repeatability uncertainty OFF. |
|
Examples |
SYST:UNC:ETER:CABL:REP ON |
|
Query Syntax |
SYSTem:UNCertainty:ETERm:CABLe:REPeat[:ENABle]? |
|
Return Type |
Boolean |
|
ON |
|
|
Applicable Models: N522xB, N523xB, N524xB (Write-Read) Sets and returns the ON/OFF state of allowing the uncertainty associated with the standard definitions in the cal kits to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty for S-Parameters. The uncertainty data for the Cal standards must also be present at the time the calibration is performed. |
|
|
Parameters |
|
|
<bool> |
Enable ON/OFF state. Choose from: ON or 1 - Standard definition uncertainty ON. OFF or 0 - Standard definition uncertainty OFF. |
|
Examples |
SYST:UNC:ETER:SDEF ON |
|
Query Syntax |
SYSTem:UNCertainty:ETERm:SDEFinitions[:ENABle]? |
|
Return Type |
Boolean |
|
ON |
|