Phase Reference Calibration


A Phase Reference calibration is performed to simplify the SMC+Phase calibration process.

Note: The phase reference cal is not required for the modulation distortion converter measurement on the E5081A. The errors are compensated automatically.

In this topic:

Other FCA Topics

Features

Requirements

Note: Do not use the U9391-60009 sine-square wave converter for E5080B and E5081A.

Note: The 67 GHz comb generator creates a large pulse for generating useful harmonics up to 67 GHz. Receiver attenuation (~ 6 dB) receiver attenuation must be used to prevent overloading the VNA receiver due to the large signal.

Limitations

How it Works

A Phase Reference Cal is performed, saved, and later recalled during a SMC Calibration. This is sometimes referred to as a 'tier 1" calibration. Due to stability of the VNA, the Phase Reference Cal can be performed infrequently. It is typically performed over the full frequency range of the VNA or Phase Reference so that it can be applied to all SMC calibrations that will be needed in the future.

The Phase Reference is a comb generator which produces signals at the multiple of its input frequency. By driving it with the VNA 10 MHz reference output, the Phase Reference produces signals at multiples of 10 MHz with a flat phase response.

During the tier 1 calibration, the VNA port 2 (B) receiver measures the phase at each 10 MHz comb frequency in order to generate correction values. These correction values are stored to a Phase Reference Cal Set which can be recalled and applied to correct subsequent SMC+Phase measurements.

Although only the B receiver is phase calibrated, an S-parameter calibration is performed at specified test ports and used to transfer the characterization to other VNA receivers.

A power calibration is also performed on port 1 as part of the Phase Reference Cal.

Unknown Mixer Calibration (extends the phase reference calibration below 650 MHz (E5080B) and 825 MHz (E5081A)

By itself, the phase reference can only be used to calibrate down to650 MHz (E5080B) and 825 MHz (E5081A) . With one additional unknown mixer connection, the phase reference calibration can be extended to the lower limit frequency which is 10 Mhz and maximum frequency range of the VNA.

With the unknown mixer process, the phase of the unknown mixer is measured as a down converter with the output frequencies set between 10 MHz and 900 MHz. By using the data acquired using the phase reference, the system is able to make produce calibrated measurements of the mixer above 650 MHz (E5080B) and 825 MHz (E5081A) . The phase response of the unknown mixer is assumed to be linear, so the expected phase response of the mixer is extrapolated down to 10 MHz. The variation in the measurements versus the expected phase response is attributed to, and used to correct, the phase response of the VNA receivers from 10 MHz to650 MHz (E5080B) and 825 MHz (E5081A) .

Unknown Mixer Properties

Hardware Setup

  1. Connect the U9391 Phase Reference to a DC power supply by one of the following cables.
    For U9391-20013 cable (2 banana plug, see the U9391 Technical Overview for more information)

For U939b. For 87405-20006 cable (3 banana plugs, see the 87405C Technical Overview for more information),

  1. Connect a cable from the VNA rear-panelReference signal output to the U9391 input. The cable should be as short as possible.

Note: Do not use the U9391-60009 sine-square wave converter for E5080B.

Note: The Reference Out is automatically set to 100 MHz during the Phase Calibration.

  1. Connect the U9391 output directly to the VNA test port 2.

  2. Insert the U9391 USB connector into any of the VNA USB ports.

 

Phase Reference Calibration Summary

The Phase Reference Cal Wizard steps will show the appropriate prompts.

 

When Unknown Mixer is enabled (Start Frequency is 10 MHz)

Phase Reference measurement above 650 MHz (E5080B) and 825 MHz (E5081A)  .

 

Full band power sensor measurement.

Full band  S-parameter Port 1 one-port calibration.

 

Full band Port 2 one-port calibration.

Full band Port1-2 thru calibration.

How to start the Phase Reference Calibration

With an Scalar Mixer / Converter + Phase measurement active...

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Cal > Main > Other Cals > Phase Reference Wizard....

  1. Click Response

  2. Select Cal

  3. Select Other Cals

  4. Select Phase Reference Wizard...

Programming Commands

 

Phase Reference Cal Settings dialog box help

Use Unknown Mixer

Check to use an Unknown Mixer to calibrate the VNA receivers below 650 MHz (E5080B) and 825 MHz (E5081A) . The Start Frequency becomes 10 MHz and can not be changed. Learn how it works.

Ports

  • Ports 1 and 2 are always selected.

  • Select port 3 and more to perform an S-parameter (SOLT) cal at those ports. The phase correction is transferred to all checked ports.

Start / Stop Frequency

Select the start and stop frequency of the Phase Reference Cal. Subsequent SMC+Phase calibrations MUST be the same or a subset of these frequencies. Interpolation is performed when the 10 MHz 'grid' of characterized frequencies is off from measurement frequencies.

  • When Unknown Mixer is NOT checked, the lowest start frequency is 650 MHz (E5080B) and 825 MHz (E5081A) . The lowest stop frequency is 1 GHz.

  • When Unknown Mixer IS checked, the start frequency is 10 MHz and can NOT be changed. The lowest stop frequency is 5 GHz.

Phase Reference

When the Phase Reference is detected by the VNA, it should appear in this field. If it does NOT appear here, try a different USB port, then click Refresh.

Phase Reference Connector type and gender. When the Phase Reference does NOT mate directly with the test port, you can add a well-behaved, broadband (no filters, waveguide, etc.) adapter to the Phase Reference and ignore it. That is because the adapter will stay with the Phase Reference and the calibration plane will still be the VNA test port connectors. The adapter adds constant delay; the deviation in delay is what is being calibrated out.  Loss in the adapter is not a concern because the adapter is not used during the S-parameter and the power meter portion of the cal.

Cal Kit Connector

Select the connector type and gender of your Cal Kit.

Only ONE connector type and gender is specified. This is because the entire Phase Reference cal is performed at the VNA test ports to reduce the effects of cable flex in the characterization.

There may be times when an adapter or connector-savers are used to connect the phase reference and cal standards to the test ports. In these cases, for highest accuracy use that adapter style and gender for ALL connections to ALL test ports. The effects of the adapter will be de-embedded automatically during subsequent SMC+Phase calibrations.

Note: For highest accuracy, the cable from test port should be as short as possible .

Cal Kit  Select the Cal Kit that will be used to perform the S-parameter Cal.

B Receiver Attenuation (E5081A)

This setting is available only when the Comb generator U9391G is used and gain coupling is off.

The 67 GHz (U9391G) phase reference outputs too much power and overloads the VNA Port 2 (B) receiver. Use at least 16 dB and not more that 20 dB of receiver attenuation to make accurate measurements using that phase reference.

This message is shown when a 67 GHz phase reference is connected to USB.

The B receiver attenuator control is shown if your VNA has receiver attenuators. Otherwise, connect external attenuation to the U9391G output when prompted.

 

Unknown Mixer Settings (Phase Reference Cal Wizard) dialog box help

The following wizard pages appear when Unknown Mixer is checked on the previous page:

Select LO source  The LO can be an internal 2nd source or an external source.

Sources  Click to start the External Devices dialog where you can select or configure an external RF source.

LO Frequency  Select a frequency that results in the unknown mixer output of 10 MHz to 900 MHz using this formula: Input = LO + Output.

Note: For best results, use the default LO frequency which avoids the VNA input (source) frequency band crossings.

  • Connect the unknown mixer input to the between port 1 and port 2. For best results, connect the mixer output as close as possible to port 2.

  • Connect the LO of the unknown mixer.  

  • Click Measure.

    • The input and output match of the unknown mixer is measured, then, SC21 using is measured.

    • The data point spacing of the calibration is decreased to 156 kHz. This point spacing is necessary to accurately characterize all the low frequency band breaks of the VNA.

 

Power Cal Settings (Phase Reference Cal Wizard) dialog box help

A power calibration is performed on port 1. This is done to simplify subsequent SMC since the power calibration will not need to be repeated.

 

 

Phase Reference Calibration Steps dialog box help

  • Connect the Phase Referenceto the port 2 test port.

    1. When using a 67 GHz phase reference, attach an attenuator (~6 dB) to the Phase Reference output .

  • Press Measure.

  • The VNA will make a series of measurements which can take several minutes:

    1. First, the match of the phase reference is measured.

    2. Then, a sweep is made at multiples of 10 MHz across the entire frequency span.

    3. An error is reported if the approximate power level is not detected.

  • 5. When finished, press Next>

Power sensor A

Connect the power sensor to port 1 test port. For above 50 GHz, due to hardware characteristics, insert a high-pass filter between the test port and power sensor.

SOLT cals are performed at the test ports.

  • The THRU standard always performs an Unknown Thru.

  • Cables (used in Phase Reference cal) or a high-pass filter (used in power cal) must be left in same place for accurate measurement.  However, an attenuator used in Phase Reference cal should be removed at this point.

  • Follow the prompts to complete the Phase Reference Cal.

Phase Ref Cal Finished

Enter a name for the Phase Ref Cal, then click Finished.

During subsequent SMC calibrations, select the Phase Reference Cal Set at the SMC Cal setup dialog. Learn more.

Specify Delay

If you know the delay value of the Unknown Thru connection, enter it here.

Otherwise, click OK to accept the calculated value.