Screen Tour


Click on image areas to learn more.

See Also


About the Touchscreen

The VNA is equipped with a 12.1-inch Hi resolution, color, touch-sensitive LCD screen for displaying traces, softkeys, and other measurement related information. The touch screen LCD allows you to make measurement settings by touching the LCD screen directly with a finger.

Important

  • Do not press the surface of the LCD screen with a sharp object such as a pen. This will damage the LCD screen surface or cause the screen to fail.

  • Occasionally, a few pixels may appear on the screen as a fixed point of blue, green or red. This is not a failure of the LCD screen and does not affect the performance of your product.

  • Because of the LCD screen, burn-in is not likely. In addition, we do not recommend using a screen-saver on the VNA.

 

How to Calibrate or turn ON | OFF the Touchscreen

Programming Commands

Using Hardkey/SoftTab/Softkey

To turn Touchscreen ON or OFF:

  1. Press Display > Display Setup.

  2. Click Touchscreen to turn ON/OFF.

The touchscreen ON |OFF setting remains until changed again from this menu, the Preferences dialog, or remotely.

Active Entry

Allows you easily select the tools. Learn more.

Trace Status

Provides details of each trace in the window. Highlighted trace indicates the active trace. Learn more.

Entry Toolbar

Along with the softkeys, allows numeric values to be entered for settings. Learn about all toolbars.

Marker Readout

Provides stimulus and response information for markers. Learn about customizing the marker readout area. See also Marker Drag.

Softkeys

The combination of hardkeys and softkeys allows easy access to all VNA features without a mouse.

SoftTabs

Pressing these tabs will display corresponding softkeys.

Hardkeys

Performs interface operations that are equivalent to those of keys in the INSTRUMENT keys, RESPONSE keys, STIMULUS keys and UTILITY keys on the front panel of VNA. Learn more.

Window Number

Provides window identification which is useful for remote programmers.

Status Bar

Provides detail about all aspects of the status of the analyzer. Learn more.

Stimulus Range

Displays the start and stop values of the sweep range.

Softkey Toolbar

These icons provide shortcuts to quickly select the softkey tools. Learn more.

Marker Drag

Drag a displayed marker across the trace using a r mouse. Learn more.

Expanded Mouse Capabilities

Windows

Traces

Markers

Softkeys

Softkey Annotations

Item

Description

Menu...

Selection launches a dialog box.

Menu

Selection launches another level of softkeys.

Item

Indicates the item (marker, trace, window) is ON. Any number of objects can be ON.

Item

Indicates the item (marker, trace, window) is OFF. Click to turn item ON.

Item

Indicates the item IS selected.

Item

Indicates the item is NOT selected. Click to select. Only one item in the collection can be ON.

* Item

Enter value in Entry toolbar.

Item
on |OFF

Capitalization indicates the current setting.