Control Auxiliary Commands


Specifies the settings to remotely control the Auxilliary IO connector.

Note: The PNA-X, N522xA and N523xA models do NOT have this connector. However, the following commands are used to control ADC voltages on the Power I/O connector: CONT:AUX:OUTP:VOLT and CONT:AUX:INPut:VOLT?.  Sending other Control:AUX commands may result in unusual behavior.

 

CONTrol:AUXiliary:

C

       | [:DATA]

       | LOGic

       | MODE

INPut

       | VOLTage?

OUTPut

       | MODE

       | VOLTage

PASSfail

       | LOGic

       | MODE

       | SCOPe

       | POLicy

       | STATus

SWEepend

   

Click on a keyword to view the command details.

 

See Also


CONTrol:AUXiliary:C[:DATA] <num>

 Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Reads and writes a 4-bit value to Port C on the Aux I/O connector. This port is connected internally to the Handler IO connector. Therefore this command will also affect the state of Port C on the Handler IO  

Parameters

 

<num>

Data value. Choose any number 0 to 15.

Examples

CONTrol:AUXiliary:C:DATA 15

For Positive Logic Port C lines C0, C1, C2, C3 go High or if in Negative Logic they go Low.

CONTrol:AUXiliary:C:DATA?

A returned value of 15 when in Positive Logic indicates Port C lines C0, C1, C2, C3 are High, or if in Negative Logic they are Low.

Query Syntax

CONTrol:AUXiliary:C:DATA?

Return Type

Numeric

Default

0


CONTrol:AUXiliary:C:LOGic <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Reads and writes the logic mode of Port C on the AUX IO. This port is connected to Port C of the Handler IO connector. Therefore, it will have the same logic setting.

Parameters

 

<char>

Logic of Port C. Choose from:

POSitive - when a value of one is written the associate line goes High.

NEGative - when a value of one is written the associate line goes Low.

When Port C is in Output/Write mode, a change in logic causes the output lines to change state immediately. For example, Low levels change to High levels.

When Port C is in Input/Read mode, a change in logic does NOT cause the lines to change, but data read from Port C will reflect the change in logic.

Examples

CONT:AUX:C:LOG POS 'Positive logic is applied to Port C data.

Query Syntax

CONTrol:AUXiliary:C:LOGic?

Return Type

Character

Default

NEGative


CONTrol:AUXiliary:C:MODE <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets Port C to read or write mode. This port is connected to Port C of the Handler IO connector. Therefore, it will have the same mode setting.

NOTE: When Port C is set to INPut mode, data writes are NOT applied to the lines. MODE must be set to OUTPut mode before writing.

Parameters

 

<char>

INPut - set the port for reading

OUTPut - set the port for writing

Examples

CONT:AUX:C:MOD INP 'set Port C to Input Mode for reading.

CONTrol:AUXiliary:C:MODE? 'queries the input/output mode that the port set to.

Query Syntax

CONTrol:AUXiliary:C:MODE?

Return Type

Character

Default

INPut


CONTrol:AUXiliary:INPut<n>:VOLTage?

Applicable Models: N522xB, N523xB, N524xB

(Read-Only)

Reads voltage on the Power I/O connector.

From the Control:Aux commands, ONLY this and CONT:AUX:OUTP:VOLT can be used on the PNA-X.

Parameters

 

<n>

Port number. If unspecified, value is set to 1.

Choose from

  • 1  Reads voltage on the AUX I/O connector (pin 14) or on the Power I/O connector Analog In 1 port (pin 7).

  • 2  Reads voltage on the Power I/O connector Analog In 2 port (pin 8).

  • 3  Reads voltage on Power I/O connector GndSens (pin 6) PNA-X only.

Examples

CONT:AUX:INPut2:VOLT?
control:auxiliary:input:voltage?

Return Type

Numeric

Default

Not Applicable


CONTrol:AUXiliary:OUTPut<n>:MODe <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) This command sets the mode of the selected "Analog Out" line on the Power I/O connector.  The modes give the user the option to have the requested voltage applied immediately or not until the sweep is done.

Parameters

 

<n>

Port number. If unspecified, value is set to 1.

<char>

WAIT - While in this mode any voltage changes sent to the selected analog out will only get applied to the output between sweeps.

NOWait - While in this mode any voltage changes sent to the selected analog out will occur right away without waiting until the end of a sweep.

Examples

CONT:AUX:OUTP1:MOD WAIT This sets the mode so that voltages sent to "Analog Out 1" are only applied at the end of a sweep.

 

CONT:AUX:OUTP2:MOD? This query returns the current mode for "Analog Out 2".

Query Syntax

CONTrol:AUXiliary:OUTPut2:MODe?

'Reads the output mode

Return Type

Character

Default

WAIT


CONTrol:AUXiliary:OUTPut<out>:VOLTage <num>

Applicable Models: N522xB, N523xB, N524xB, E5080B, E5081A

(Read-Write)

Sets and reads voltage on the Power I/O connector AnalogOut1|2 (PNA), AUX Out 1|2 (E5080B, E5081A).

(PNA) From the Control:Aux commands, ONLY this and CONT:AUX:INPut:VOLT? can be used.

Parameters

 

<out>

DAC output number. Choose from:

1 - PNA: Output 1 (Aux I/O pin 3) and (Power I/O pin 3), E5080B AUX Out 1

2 - PNA: Output 2 (Aux I/O pin 2) and (Power I/O pin 4), E5080B AUX Out 2

<num>

Output Voltage. Choose a voltage value between -10 and +10 volts

Examples

CONT:AUX:OUTP1:VOLT 5
control:auxiliary:output2:voltage 5

Query Syntax

CONTrol:AUXiliary:OUTPut<out>:VOLTage?

'Reads the output DAC voltage

Return Type

Numeric

Default

0


CONTrol:AUXiliary:PASSfail:LOGic <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets the logic of the PassFail line (pin 12) on the Material Handler IO (pin 33).

Parameters

 

<char>

Choose from:
POSitive
- Causes the PassFail line to have positive logic (high = pass, low = fail).

NEGative - Causes the PassFail line to have negative logic (high = fail, low = pass).

Examples

CONT:AUX:PASS:LOG POS
control:auxiliary:passfail:logic negative

Query Syntax

CONTrol:AUXiliary:PASSfail:LOGic?

Return Type

Character

Default

POSitive


CONTrol:AUXiliary:PASSfail:MODe <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets and reads the default logical pass/fail state. This is the state the pass/fail line stays in until a failure occurs (if the mode is NOWait), or until an end-of-sweep condition occurs (if the modes is PASS or FAIL).

The end-of-sweep condition is determined by the CONTrol:AUXiliary:PASSfail:SCOPe command.

Parameters

 

<char>

Choose from:
PASS
- the line stays in PASS state until the end-of-sweep condition occurs, at which time the pass/fail line is set, and the pass/fail strobe (line 36) is activated.

FAIL - the line stays in FAIL state until the end-of-sweep condition occurs, at which time the pass/fail line is set, and the pass/fail strobe (line 36) is activated.

NOWait - the pass/fail line is set, and the pass/fail strobe (line 36) is activated as soon as a failure condition occurs.

Examples

CONT:AUX:PASS:MODE NOW
control:auxiliary:passfail:mode fail

Query Syntax

CONTrol:AUXiliary:PASSfail:MODE?

Return Type

Character

Default

NOWait


CONTrol:AUXiliary:PASSfail:SCOPe <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets and reads the scope of pass/fail testing. The pass/fail line can report the status of all measurements on each channel, or all measurements on all channels. This command selects which option to use.

Parameters

 

<char>

Choose from:

CHANnel - A pass/fail result is computed and written to the output pins at the end of all sweeps on a channel.

GLOBal - A pass/fail result is computed and written to the output pins at the end of all sweeps on a channel.

If the pass/fail mode is NOWait (as set by CONTrol:AUXiliary:PASSfail:MODe), the status and strobe pins are written immediately. Otherwise the pins are written as indicated above. Regardless of the mode value, the pass/fail line is returned to its default state (as set by the MODE command) at the end of channel or group of channels.

Examples

CONT:AUX:PASS:SCOP CHAN
control:auxiliary:passfail:scope sweep

Query Syntax

CONTrol:AUXiliary:PASSfail:SCOPe?

Return Type

Character

Default

GLOBal


CONTrol:AUXiliary:PASSfail:POLicy <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets the policy used to determine how global pass/fail is computed.

Parameters

 

<char>

Name of the policy to use. Choose from:

ALLTests - Pass/Fail Status returns PASS if all tests on all measurements pass.

ALLMeas  - Pass/Fail Status returns PASS if all measurements have associated tests, and all tests pass. FAIL is returned if even one measurement has no associated limit test.

Only those measurements which are not in HOLD mode contribute to the pass/fail result.

Examples

CONT:AUX:PASS:POL ALLM
control:auxiliary:passfail:policy alltests

Query Syntax

CONTrol:AUXiliary:PASSfail:POLicy?

Return Type

Character

Default

ALLTests


CONTrol:AUXiliary:PASSfail:STATus?

Applicable Models: N522xB, N523xB, N524xB

(Read-Only) Returns the most recent pass/fail status value. Use this command as follows:

  1. Set the VNA trigger scope to ALL

  2. Set the VNA trigger source to MANUAL or EXTERNAL.

  3. Trigger the VNA.

  4. Use the *OPC? command to determine when the sweep is complete.

  5. Use the CONT:AUX:PASS:STAT? query to obtain the global pass/fail result.

Return Type

Character - One of the following is returned:

PASS - all measurements not in HOLD mode have been swept, and all associated limit tests have passed.

FAIL - all measurements not in HOLD mode have been swept, and one or more limit tests failed according to the specified Pass/Fail policy.

NONE - status cannot be determined because measurements are in progress.

Default

Not Applicable


CONTrol:AUXiliary:SWEepend <char>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Specifies the event that will cause the Sweep End line pin 11) to go to a low (false) state of the Material Handler IO.  The line will return to a high state after the appropriate calculations are complete.

Parameters

 

<char>

Choose from:
SWEep -
the line goes low when each sweep is complete.

CHANnel - The line goes low when all of the sweeps for each channel is complete.

GLOBal - The  line goes low when all the sweeps for all channels are complete.

Examples

CONT:AUX:SWE SWE
control:auxiliary:sweepend channel

Query Syntax

CONTrol:AUXiliary:SWEepend?

Return Type

Character

Default

SWEep